<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FXOS8700 magnetic interrupt in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705823#M4548</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented thefirst snippet without the asleep configuration and indeed it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is with the&amp;nbsp;&lt;/P&gt;&lt;PRE class=""&gt;&lt;CODE&gt;M_THS_COUNT_REG&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;which determines the debouncing interval. Specifically the interrupt triggers very late with regards to the project requirements. Initially this was set to 1.&lt;/P&gt;&lt;P&gt;Would this sensor work, assuming you have to track very fast moving object such as cars. (transient magnetic fields)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet suggests the minimum time is 20ms but from experimental results the delay is much larger than that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Di&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2017 13:26:22 GMT</pubDate>
    <dc:creator>diken</dc:creator>
    <dc:date>2017-09-20T13:26:22Z</dc:date>
    <item>
      <title>FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705818#M4543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to configure the FXOS8700CQR in magnetic threshold interrupt mode. I am using SPI to communicate witth the sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whenever a magnet is in the vicinity of the sensor, the programmed magnetic threshold values is supposed to trigger an interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the data is streaming I can clearly see the spikes on the signal passing the programmed threshold.&lt;/P&gt;&lt;P&gt;The interrupt pin does not go high however. I checked with a scope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see the magnetic interrupts happening.The problem is that the magnetic interrupts in the ISR are not triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even if I trigger them manually by the shaking the unit I cannot clear them. Pin stays always high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any application note with regard to the magnetic threshold interrupt specifically. (not the vector magnitude)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FXOS8700CQ_ConfigMagTHS&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;MAG_RST_HIGH&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Hard Reset , RST active HIGH&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__delay_ms&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;MAG_RST_LOW&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;__delay_ms&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 

&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;CTRL_REG2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; SMOD_LOW_NOISE&lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;SLPE_MASK&lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;MOD_LOW_NOISE&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Low noise, low power, auto-sleep mode enabled&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;CTRL_REG3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; IPOL_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Active HIGH on INT, push-pull mode&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;CTRL_REG4&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// No interrupt enabled here&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;CTRL_REG5&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// No interrupt routed to pin 2&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;ASLP_COUNT&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x05&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// 20 ms -&amp;nbsp; if not interrupt is asserted in 20 ms the system will go back to sleep mode&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_ACAL_MASK&lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_OSR_50_HZ &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_HMS0_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//&amp;nbsp; automatic calibration,&amp;nbsp; one shot magnetic reset, only mag active&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_CTRL_REG2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_MAXMIN_DIS_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_MAXMIN_DIS_THS_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_MAXMIN_RST_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; RST_DISABLED&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//Magnetic min/max enabled&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_CTRL_REG3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_ASLP_OSR_100_HZ &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_XYZ_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_ST_Z_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_ST_XY_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// all updated when THS ISR happens&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;

&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_CFG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_ELE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_OAE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_WAKE_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_ZEFE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_YEFE &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_XEFE&lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_WAKE_EN &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; M_THS_INT_EN &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;//M_INT_threshold on INT2 pin&amp;nbsp; OR INT of all axes for threshold, latch disabled.&lt;/SPAN&gt;

uint16_t magThreshold &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x200&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//counts;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
uint8_t magThresholdHi &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;gt;&amp;gt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
uint8_t magThresholdLo &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_Z_MSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdHi&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Debounce countered cleared to zero when threshold is not longer true&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_Z_LSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdLo&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; 
magThreshold &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x200&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//counts;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
magThresholdHi &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;gt;&amp;gt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
magThresholdLo &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_X_MSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdHi&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Debounce countered cleared to zero when threshold is not longer true&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_X_LSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdLo&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
 
magThreshold &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x200&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;//counts;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
magThresholdHi &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;gt;&amp;gt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
magThresholdLo &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; magThreshold &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xFF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_Y_MSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdHi&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Debounce countered cleared to zero when threshold is not longer true&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_Y_LSB&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; magThresholdLo&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_COUNT&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//debounce sample counts required before a magnetic threshold event is triggered, depends on ODR &lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;FXOS8700CQ_WriteByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; ASLP_RATE_20MS &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; DATA_RATE_100HZ &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;LNOISE_MASK &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;// in sleep mode data rate 50Hz, awake ODR = 100Hz, low noise mode, in standby&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code above is executed between:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="token function"&gt;FXOS8700CQ_StandbyMode&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

&lt;SPAN class="token function"&gt;FXOS8700CQ_ActiveMode&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the interrupt I try to clear the interrupt and in the main () function I try to print the source but I don't see anything at all.&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="token function"&gt;_INTInterrupt&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
MagTHSEvent &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
magintsrc &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FXOS8700CQ_ReadByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_INT_SRC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
 &lt;SPAN class="comment token"&gt;//Read interrupt source to clear int&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
srcmag &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FXOS8700CQ_ReadByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_THS_SRC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp; 
magintsrc &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;FXOS8700CQ_ReadByte&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;M_INT_SRC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
 &lt;SPAN class="comment token"&gt;//Read interrupt source to clear int&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//Clear the INT interrupt flag &lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705818#M4543</guid>
      <dc:creator>diken</dc:creator>
      <dc:date>2026-02-03T21:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705819#M4544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to reproduce your settings and get back to you soon. At first glance everything seems to be correct. Can you please try to test the magnetometer threshold function without using the sleep mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 13:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705819#M4544</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-09-18T13:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705820#M4545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already tried disabling the sleep mode with the same results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sleep mode functionality is needed however since this is&amp;nbsp; a long term solution where you can't easily replace the batteries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried changing the threshold on z axis. Still the same issue.&lt;/P&gt;&lt;P&gt;When a magnetic object (ex headphone) is in the vicinity all 3 axis are above 100 counts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As it stands right now the magnetometer streams data correctly however the interrupt functionality is not responsive and does not change as per spec even if taking into account the debouncing counter (M_THS_COUNT)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Di&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 21:42:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705820#M4545</guid>
      <dc:creator>diken</dc:creator>
      <dc:date>2017-09-18T21:42:08Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705821#M4546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Di,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have just done a simple test using the following settings (without the sleep mode) and it works well as you can see on the picture below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; FXOS8700CQ_Init &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_X_MSB_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Threshold value MSB&amp;nbsp; &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_X_LSB_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Threshold value LSB&amp;nbsp; &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_CFG_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xCB&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Event flag latch enabled, logic OR of enabled axes, only X-axis enabled, threshold interrupt enabled and routed to INT1 &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_COUNT_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// 100ms at 100Hz ODR and magnetometer mode only &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x1D&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Max OSR, only magnetometer is active &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Push-pull, active low interrupt &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x19&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// ODR = 100Hz, Active mode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;PORTD_IRQHandler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTD_PCR4 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORT_PCR_ISF_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Clear the interrupt flag &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; M_Ths_Source &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;I2C_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_SRC_REG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Read the M_THS_SRC register to clear the SRC_M_THS flag in the M_INT_SRC register and deassert the INT1 pin&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="Mag threshold.JPG"&gt;&lt;IMG alt="Mag threshold.JPG" src="https://community.nxp.com/t5/image/serverpage/image-id/31416i6C1787CE1EA929B2/image-size/large?v=v2&amp;amp;px=999" title="Mag threshold.JPG" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please try to reproduce it? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Meanwhile I will try to implement the sleep mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705821#M4546</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2020-11-02T14:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705822#M4547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Di,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I successfully implemented the sleep mode, here is my code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; FXOS8700CQ_Init &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_X_MSB_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Threshold value MSB&amp;nbsp; &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_X_LSB_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Threshold value LSB&amp;nbsp; &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_CFG_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0xCF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Event flag latch enabled, logic OR of enabled axes, only X-axis enabled, wake on magnetic threshold event, threshold interrupt enabled and routed to INT1 &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_COUNT_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0A&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// 100ms at 100Hz ODR and magnetometer mode only &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x1D&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Max OSR, only magnetometer is active &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Push-pull, active low interrupt &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG2&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x04&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Auto-sleep mode enabled&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; ASLP_COUNT_REG&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x06&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Auto-sleep counter set to 1.92s (6 x 0.32s = 1.92s) &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG4&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Auto-sleep/wake interrupt enabled&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG5&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Route auto-sleep/wake interrupt to INT1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;I2C_WriteRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; CTRL_REG1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x19&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// ODR = 100Hz, Active mode&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;PORTD_IRQHandler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTD_PCR4 &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORT_PCR_ISF_MASK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Clear the interrupt flag &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Int_Flag &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; 
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;Int_Flag&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Int_Flag &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Int_Source &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;I2C_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_INT_SRC_REG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;Int_Source &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x04&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Magnetic threshold event detected?&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; M_Ths_Src &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;I2C_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; M_THS_SRC_REG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Read the M_THS_SRC register to clear the SRC_M_THS flag in the M_INT_SRC register and deassert the INT1 pin&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Event_Counter&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Int_Source &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;I2C_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; INT_SOURCE_REG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;Int_Source &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;// Auto-sleep/wake interrupt?&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sysmod &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;I2C_ReadRegister&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;FXOS8700CQ_I2C_ADDRESS&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; SYSMOD_REG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it will help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 12:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705822#M4547</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-09-20T12:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705823#M4548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented thefirst snippet without the asleep configuration and indeed it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is with the&amp;nbsp;&lt;/P&gt;&lt;PRE class=""&gt;&lt;CODE&gt;M_THS_COUNT_REG&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;which determines the debouncing interval. Specifically the interrupt triggers very late with regards to the project requirements. Initially this was set to 1.&lt;/P&gt;&lt;P&gt;Would this sensor work, assuming you have to track very fast moving object such as cars. (transient magnetic fields)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet suggests the minimum time is 20ms but from experimental results the delay is much larger than that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Di&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 13:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705823#M4548</guid>
      <dc:creator>diken</dc:creator>
      <dc:date>2017-09-20T13:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705824#M4549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Di,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The time step used by the debounce counter depends on the chosen ODR and m_hms[1:0] bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_17.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32065i8DE18177E4C12E40/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_17.png" alt="pastedImage_17.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the only way to reduce the time step is to increase the ODR and eventually use only the magnetometer (m_hms[1:0] = 0b01).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 06:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/705824#M4549</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-09-21T06:59:55Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/1504118#M7029</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/113286"&gt;@diken&lt;/a&gt;&amp;nbsp;or&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12216"&gt;@TomasVaverka&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking to do a similar thing - count cars and I have some FXOS8700OS devices on-hand. &amp;nbsp;Is there an example of using the hardware interrupt for magnetic threshold detection I could use as a staring point? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Chip&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 15:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/1504118#M7029</guid>
      <dc:creator>chipmc</dc:creator>
      <dc:date>2022-08-10T15:41:33Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 magnetic interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/1666675#M7462</link>
      <description>&lt;P&gt;Hello, were you able to carry out your project, I have a similar project, could you help me?&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jun 2023 06:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-magnetic-interrupt/m-p/1666675#M7462</guid>
      <dc:creator>alexmv24</dc:creator>
      <dc:date>2023-06-09T06:13:46Z</dc:date>
    </item>
  </channel>
</rss>