<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FXOS8700CQ - lnoise in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-lnoise/m-p/705455#M4542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Efthymios,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the datasheet when the full-scale range is set to 2g, the measurement range is –2 g to +1.999 g, and each count corresponds to 0.244 mg at ±14-bits resolution and it's not affected for the low noise mode. Also, the low-noise accelerometer mode works independently of the oversampling modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Oct 2017 22:55:29 GMT</pubDate>
    <dc:creator>darioarias</dc:creator>
    <dc:date>2017-10-18T22:55:29Z</dc:date>
    <item>
      <title>FXOS8700CQ - lnoise</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-lnoise/m-p/705454#M4541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;In register&amp;nbsp; &lt;SPAN class=""&gt;CTRL_REG1&lt;/SPAN&gt;&amp;nbsp;of the FXOS8700CQ acceleration sensor, there is the option lnoise. The manual states the following...&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Reduced noise and full-scale range mode (analog gain times 2).&lt;BR /&gt;0 – Normal mode&lt;BR /&gt;1 – Reduced noise mode; Note that the FSR setting is restricted to ±2 g or ±4 g mode. This feature&lt;BR /&gt;cannot be used in ±8 g mode.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When arming that bit at a range of +-2g, is the resolution of&amp;nbsp; &lt;SPAN class=""&gt;0.244 mg/LSB&amp;nbsp;stays the same or it is being halved (0.122 mg/LSB)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Does this reduced noise mode has to do anything with oversampling (OSR)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700CQ-lnoise/m-p/705454#M4541</guid>
      <dc:creator>ekalyvio</dc:creator>
      <dc:date>2026-02-03T22:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700CQ - lnoise</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700CQ-lnoise/m-p/705455#M4542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Efthymios,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the datasheet when the full-scale range is set to 2g, the measurement range is –2 g to +1.999 g, and each count corresponds to 0.244 mg at ±14-bits resolution and it's not affected for the low noise mode. Also, the low-noise accelerometer mode works independently of the oversampling modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2017 22:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700CQ-lnoise/m-p/705455#M4542</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-10-18T22:55:29Z</dc:date>
    </item>
  </channel>
</rss>