<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Oversampling - FXOS8700CQ</title>
    <link>https://community.nxp.com/t5/Sensors/Oversampling-FXOS8700CQ/m-p/703010#M4537</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Efthymios,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OSR determines the number of averaged samples. As you correctly stated, at an ODR of 100Hz and OSR = 7, 16 samples are gathered (the sampling rate is actually 1600Hz) and averaged. Table 203 summarizes all eight oversampling options which trade-off between resolution and current consumption at varying sample rates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30099i72C6056FC6579D6A/image-size/large?v=v2&amp;amp;px=999" title="Table 203.JPG" alt="Table 203.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Oct 2017 14:12:38 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2017-10-12T14:12:38Z</dc:date>
    <item>
      <title>Oversampling - FXOS8700CQ</title>
      <link>https://community.nxp.com/t5/Sensors/Oversampling-FXOS8700CQ/m-p/703009#M4536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What exactly is Oversampling Rate (OSR)? If for example I set an ODR of 100 Hz for the magnetometer at an OSR=7, does this mean that the magnetometer will gather 16 samples, process them somehow and of all these 16 samples will return 1 as an output? What kind of processing is happening? (eg. Is it used any kind of averaging function?) Is oversampling having some kind of latency in the data (meaning that for a movement, we have some kind of hysteresis until we detect it)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Oversampling-FXOS8700CQ/m-p/703009#M4536</guid>
      <dc:creator>ekalyvio</dc:creator>
      <dc:date>2026-02-03T22:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: Oversampling - FXOS8700CQ</title>
      <link>https://community.nxp.com/t5/Sensors/Oversampling-FXOS8700CQ/m-p/703010#M4537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Efthymios,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OSR determines the number of averaged samples. As you correctly stated, at an ODR of 100Hz and OSR = 7, 16 samples are gathered (the sampling rate is actually 1600Hz) and averaged. Table 203 summarizes all eight oversampling options which trade-off between resolution and current consumption at varying sample rates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30099i72C6056FC6579D6A/image-size/large?v=v2&amp;amp;px=999" title="Table 203.JPG" alt="Table 203.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 14:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Oversampling-FXOS8700CQ/m-p/703010#M4537</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-10-12T14:12:38Z</dc:date>
    </item>
  </channel>
</rss>