<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: FXTH87 Datasheet Typo</title>
    <link>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691453#M4465</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lucas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No this is not a contradiction: this means the PIN bit will be set in STOP1 due to an active-low level on the external reset pin only &lt;STRONG&gt;if the external reset pin is pulled high&lt;/STRONG&gt;. If the pin is pulled low then the PIN bit will not be set after an active-low level on the external pin in STOP1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need more clarification, please let us know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 May 2017 10:40:54 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2017-05-29T10:40:54Z</dc:date>
    <item>
      <title>FXTH87 Datasheet Typo</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691452#M4464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;Page 38, Table 25.&lt;/EM&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;External Reset Pin&lt;/STRONG&gt; —&lt;/P&gt;&lt;P&gt;This bit indicates reset was caused by an active-low level on the external reset pin if the device was in either the &lt;STRONG&gt;STOP1&lt;/STRONG&gt; or RUN modes. This bit is not set if the external reset pin is pulled low when the device is in the &lt;STRONG&gt;STOP1&lt;/STRONG&gt; mode.&lt;BR /&gt;0 Reset not caused by external reset pin&lt;BR /&gt;1 Reset came from external reset pin&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Sentence&lt;/STRONG&gt;&lt;STRONG&gt;&amp;nbsp;One Says:&lt;/STRONG&gt; Bit &lt;SPAN style="text-decoration: underline;"&gt;is set&lt;/SPAN&gt; in Stop1 Mode.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Sentence Two Says:&lt;/STRONG&gt; Bit &lt;SPAN style="text-decoration: underline;"&gt;is NOT set&lt;/SPAN&gt; in Stop1 Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sentence two contradicts sentence one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which is it? Both of these sentences cannot be true.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691452#M4464</guid>
      <dc:creator>lucascooter</dc:creator>
      <dc:date>2026-02-03T23:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: FXTH87 Datasheet Typo</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691453#M4465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lucas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No this is not a contradiction: this means the PIN bit will be set in STOP1 due to an active-low level on the external reset pin only &lt;STRONG&gt;if the external reset pin is pulled high&lt;/STRONG&gt;. If the pin is pulled low then the PIN bit will not be set after an active-low level on the external pin in STOP1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need more clarification, please let us know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 May 2017 10:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691453#M4465</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-05-29T10:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: FXTH87 Datasheet Typo</title>
      <link>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691454#M4466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see the word "high" written anywhere. Could you give me examples of scenarios where there bit is and is not set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scenario 1: MCU is in STOP1 mode, user presses reset button which pulls the reset pin low momentarily and wakes up the MCU. Is the bit set to 1 or is it not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 16:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXTH87-Datasheet-Typo/m-p/691454#M4466</guid>
      <dc:creator>lucascooter</dc:creator>
      <dc:date>2017-05-30T16:34:33Z</dc:date>
    </item>
  </channel>
</rss>