<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Memory and flash requirements for Sensor Fusion</title>
    <link>https://community.nxp.com/t5/Sensors/Memory-and-flash-requirements-for-Sensor-Fusion/m-p/683308#M4422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I picked as an example the project FSFK-K64F for the sensor fusion and after compiling it gave me the following results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; text&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; data&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bss&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dec&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; hex&amp;nbsp;&amp;nbsp; &amp;nbsp;filename&lt;BR /&gt;&amp;nbsp; 79244&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 64&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 20708&amp;nbsp;&amp;nbsp; &amp;nbsp; 100016&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 186b0&amp;nbsp;&amp;nbsp; &amp;nbsp;FSFK_K64F.elf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash memory or the SRAM are not nearly enough for running e-Compass Algorithms, my recommendation would be to strictly pick only what you need from the code, because this code is meant to run a GUI that shows the values of the sensor in real time.&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jun 2017 20:07:05 GMT</pubDate>
    <dc:creator>darioarias</dc:creator>
    <dc:date>2017-06-02T20:07:05Z</dc:date>
    <item>
      <title>Memory and flash requirements for Sensor Fusion</title>
      <link>https://community.nxp.com/t5/Sensors/Memory-and-flash-requirements-for-Sensor-Fusion/m-p/683307#M4421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a board with CPU/Flash/RAM that is similar to the Kinetis platforms:&lt;/P&gt;&lt;P&gt;48Mhz ARM CPU,128 KB flash and 16 KB SRAM&lt;/P&gt;&lt;P&gt;However the operating system takes up most of that&lt;/P&gt;&lt;P&gt;My build (without the Sensor Fusion library) produces the following message:&lt;/P&gt;&lt;P&gt;Flash used: 114033 of 131072 bytes (87.0 %).&lt;BR /&gt;SRAM used: 14144 of 16384 bytes (86.3 %). Stack: 2048 bytes. Heap: 1024 bytes.&lt;/P&gt;&lt;P&gt;Is what I have left that enough to run sensor fusion e-Compass algorithm ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Memory-and-flash-requirements-for-Sensor-Fusion/m-p/683307#M4421</guid>
      <dc:creator>heelcurve5</dc:creator>
      <dc:date>2026-02-03T22:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: Memory and flash requirements for Sensor Fusion</title>
      <link>https://community.nxp.com/t5/Sensors/Memory-and-flash-requirements-for-Sensor-Fusion/m-p/683308#M4422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I picked as an example the project FSFK-K64F for the sensor fusion and after compiling it gave me the following results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; text&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; data&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bss&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dec&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; hex&amp;nbsp;&amp;nbsp; &amp;nbsp;filename&lt;BR /&gt;&amp;nbsp; 79244&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 64&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 20708&amp;nbsp;&amp;nbsp; &amp;nbsp; 100016&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; 186b0&amp;nbsp;&amp;nbsp; &amp;nbsp;FSFK_K64F.elf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash memory or the SRAM are not nearly enough for running e-Compass Algorithms, my recommendation would be to strictly pick only what you need from the code, because this code is meant to run a GUI that shows the values of the sensor in real time.&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2017 20:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Memory-and-flash-requirements-for-Sensor-Fusion/m-p/683308#M4422</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-06-02T20:07:05Z</dc:date>
    </item>
  </channel>
</rss>