<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pressure sensor for water in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675666#M4370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. I will read these application notes :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jul 2017 07:56:37 GMT</pubDate>
    <dc:creator>mortencomadan</dc:creator>
    <dc:date>2017-07-25T07:56:37Z</dc:date>
    <item>
      <title>Pressure sensor for water</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675664#M4368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for a pressure sensor that can have measure the pressure of water directy applied to the sensor.&lt;/P&gt;&lt;P&gt;The pressure i want to measure is maximum 2bar absolute or 1 bar differential. It only really needs one port.&lt;/P&gt;&lt;P&gt;But it has to fit a silicone tube tha has a &amp;nbsp;innner diameter of around 5-6mm. It is not super critical though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675664#M4368</guid>
      <dc:creator>mortencomadan</dc:creator>
      <dc:date>2026-02-03T22:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure sensor for water</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675665#M4369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Morten,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;We do not recommend all our sensor to become in direct contact with any kind of liquid substance or corrosive gases which would damage the gel and cause the sensor to become out of specification. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;However, our products are used in washing machine applications, which would expose the gel to a humid environment. In these applications, the device is located at the top of a measurement tube - so water level is indirectly measured through the water pushing a trapped air column up to the sensor. As you can see in the following application notes, the sensor does not have a direct contact with water, but is separated by the air column.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf"&gt;http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;AN1950: Water Level Monitoring&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;&lt;A href="http://www.freescale.com/files/sensors/doc/app_note/AN1516.pdf"&gt;AN1516: Liquid Level Control Using a Pressure Sensor&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;&lt;A href="http://www.freescale.com/files/sensors/doc/app_note/AN3728.pdf"&gt;AN3728: Media Compatibility for IPS PRT Pressure Sensors&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;Our sensors come in differential, gauge or absolute configuration and the sensors that can handle up t 1 bar are the &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-1000-kpa/differential-gauge-and-absolute-pressure-sensor-0-to-200kpa:MPXx2200"&gt;MPXx2200&lt;/A&gt; or &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/differential-gauge-up-to-1000-kpa/differential-gauge-and-absolute-pressure-sensor-0-to-200kpa:MPXx2202"&gt;MPXx2202.&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;Hope it helps!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif;"&gt;Darío&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 20:27:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675665#M4369</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-07-24T20:27:12Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure sensor for water</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675666#M4370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. I will read these application notes :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 07:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-for-water/m-p/675666#M4370</guid>
      <dc:creator>mortencomadan</dc:creator>
      <dc:date>2017-07-25T07:56:37Z</dc:date>
    </item>
  </channel>
</rss>