<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Sensor MPX2300DT1 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Sensor-MPX2300DT1/m-p/675239#M4367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joerg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;There is no documentation that certifies that the production of this part is made under clean room conditions and the part is no sterilized after production .This device have been designed with bio-medically approved materials with a history in medical situations to provide a sensor that can be used with confidence in applications, such as invasive blood pressure monitoring. It can be sterilized using ethylene oxide and it&lt;SPAN style="font-size: small;"&gt; meets all USP XX Biological Testing Class VI requirements.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 23:29:34 GMT</pubDate>
    <dc:creator>darioarias</dc:creator>
    <dc:date>2017-07-24T23:29:34Z</dc:date>
    <item>
      <title>Sensor MPX2300DT1</title>
      <link>https://community.nxp.com/t5/Sensors/Sensor-MPX2300DT1/m-p/675238#M4366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the Freescale Pressure Sensor MPX2300DT1 produced and packed under clean room conditions? Which class of cleanroom? Is the sensor sterilized after production? Do you have any document, that cerifies the cleanroom production?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Sensor-MPX2300DT1/m-p/675238#M4366</guid>
      <dc:creator>joergmeier</dc:creator>
      <dc:date>2026-02-03T23:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: Sensor MPX2300DT1</title>
      <link>https://community.nxp.com/t5/Sensors/Sensor-MPX2300DT1/m-p/675239#M4367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joerg,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;There is no documentation that certifies that the production of this part is made under clean room conditions and the part is no sterilized after production .This device have been designed with bio-medically approved materials with a history in medical situations to provide a sensor that can be used with confidence in applications, such as invasive blood pressure monitoring. It can be sterilized using ethylene oxide and it&lt;SPAN style="font-size: small;"&gt; meets all USP XX Biological Testing Class VI requirements.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 23:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Sensor-MPX2300DT1/m-p/675239#M4367</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-07-24T23:29:34Z</dc:date>
    </item>
  </channel>
</rss>