<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Need help in selecting a Sensor</title>
    <link>https://community.nxp.com/t5/Sensors/Need-help-in-selecting-a-Sensor/m-p/674029#M4359</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radhesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The portfolio of low-power touch sensors use the human body as one of the capacitive plates of an electrical circuit.&amp;nbsp; Capacitive sensors can also switch without contact due to proximity sensing or used with external plates connected to the device. I think this type of sensor are suitable for your application where the external plate is shaped as a continent. The sensors we have are, &lt;A href="http://cache.nxp.com/docs/en/data-sheet/PCF8883.pdf"&gt;PCF8883&lt;/A&gt; and &lt;A href="http://cache.nxp.com/docs/en/data-sheet/PCF8885.pdf"&gt;PCF8885&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope you found them useful&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Jun 2017 21:05:40 GMT</pubDate>
    <dc:creator>darioarias</dc:creator>
    <dc:date>2017-06-30T21:05:40Z</dc:date>
    <item>
      <title>Need help in selecting a Sensor</title>
      <link>https://community.nxp.com/t5/Sensors/Need-help-in-selecting-a-Sensor/m-p/674028#M4358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, For my Mater thesis I am developing an Interactive Globe, for which I require a sensor which can sense TOUCH. The user will be touching a continent and this should result in stating the respective name of the continent. The problem I am facing is that the user won't be touching the sensor directly. Can anybody suggest a sensor for this application???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:06:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Need-help-in-selecting-a-Sensor/m-p/674028#M4358</guid>
      <dc:creator>radheshpulimutt</dc:creator>
      <dc:date>2026-02-03T23:06:23Z</dc:date>
    </item>
    <item>
      <title>Re: Need help in selecting a Sensor</title>
      <link>https://community.nxp.com/t5/Sensors/Need-help-in-selecting-a-Sensor/m-p/674029#M4359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radhesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The portfolio of low-power touch sensors use the human body as one of the capacitive plates of an electrical circuit.&amp;nbsp; Capacitive sensors can also switch without contact due to proximity sensing or used with external plates connected to the device. I think this type of sensor are suitable for your application where the external plate is shaped as a continent. The sensors we have are, &lt;A href="http://cache.nxp.com/docs/en/data-sheet/PCF8883.pdf"&gt;PCF8883&lt;/A&gt; and &lt;A href="http://cache.nxp.com/docs/en/data-sheet/PCF8885.pdf"&gt;PCF8885&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope you found them useful&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 21:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Need-help-in-selecting-a-Sensor/m-p/674029#M4359</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-06-30T21:05:40Z</dc:date>
    </item>
  </channel>
</rss>