<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bi-directional Pressure Sensor in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Bi-directional-Pressure-Sensor/m-p/670948#M4342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using the MP3V5050. Is there any sensor that can perform both negative and positive &amp;nbsp;pressure measurements from the same chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can an absolute sensor measure both?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:48:02 GMT</pubDate>
    <dc:creator>jaredweldon</dc:creator>
    <dc:date>2026-02-03T21:48:02Z</dc:date>
    <item>
      <title>Bi-directional Pressure Sensor</title>
      <link>https://community.nxp.com/t5/Sensors/Bi-directional-Pressure-Sensor/m-p/670948#M4342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using the MP3V5050. Is there any sensor that can perform both negative and positive &amp;nbsp;pressure measurements from the same chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can an absolute sensor measure both?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Bi-directional-Pressure-Sensor/m-p/670948#M4342</guid>
      <dc:creator>jaredweldon</dc:creator>
      <dc:date>2026-02-03T21:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Bi-directional Pressure Sensor</title>
      <link>https://community.nxp.com/t5/Sensors/Bi-directional-Pressure-Sensor/m-p/670949#M4343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jared,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We do have a few pressure sensors that can handle both negative pressure and positive pressure without resulting in damage in the device. This sensors are &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-2-to-2kpa-vacuum-pressure-sensor:MPXV7002?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;MPXV7002&lt;/A&gt; (-2 kPa / +2 kPa), &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-7-to-7kpa-differential-and-gauge-pressure-sensor:MPXV7007DP?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;MPXV7007&lt;/A&gt; (-7 kPa/ +7 kPa) and &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/vacuum-sensors-50-to-115-kpa/-25-to-25kpa-differential-and-gauge-pressure-sensor:MPXV7025DP?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;MPXV7025&lt;/A&gt; (-25 kPa/25 kPa).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Absolute pressure sensors cannot measure negative pressure, because they are meant to measure the environment's pressure which is always positive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2017 19:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Bi-directional-Pressure-Sensor/m-p/670949#M4343</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-07-18T19:54:22Z</dc:date>
    </item>
  </channel>
</rss>