<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMPX2010 minimum supply voltage</title>
    <link>https://community.nxp.com/t5/Sensors/MPX2010-minimum-supply-voltage/m-p/649402#M4119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPX2010 defined&amp;nbsp;supply voltages typ.10V and&amp;nbsp;maximum 16V, however it did not defined minimum supply voltage.&lt;/P&gt;&lt;P&gt;Could you tell me it minimum supply voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;M.Kiniwa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:56:35 GMT</pubDate>
    <dc:creator>masahirokiniwa</dc:creator>
    <dc:date>2026-02-03T22:56:35Z</dc:date>
    <item>
      <title>MPX2010 minimum supply voltage</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010-minimum-supply-voltage/m-p/649402#M4119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPX2010 defined&amp;nbsp;supply voltages typ.10V and&amp;nbsp;maximum 16V, however it did not defined minimum supply voltage.&lt;/P&gt;&lt;P&gt;Could you tell me it minimum supply voltage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;M.Kiniwa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010-minimum-supply-voltage/m-p/649402#M4119</guid>
      <dc:creator>masahirokiniwa</dc:creator>
      <dc:date>2026-02-03T22:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPX2010 minimum supply voltage</title>
      <link>https://community.nxp.com/t5/Sensors/MPX2010-minimum-supply-voltage/m-p/649403#M4120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello M.Kiniwa,&lt;/P&gt;&lt;P&gt;Thank you for writing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, the MPX2010 is ratiometric to supply voltage.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The typical supply voltage is 10 volts and the specifications as noted on the data sheet are at 10 volts supply.&amp;nbsp; At 5 volts, for example, the device will operate as this is within the 0 to 16v range for the supply voltage.&amp;nbsp; The only difference being the change in full scale span will be ratiometric to the change in supply voltage.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can reduce the supply voltage and therefore, the full-scale output of the sensor will change linearly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Theoretical supply voltage can be close to zero voltage but absolute errors would be highest then measured. I recommend using at least 2V supply because of mentioned reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 16:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX2010-minimum-supply-voltage/m-p/649403#M4120</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2017-04-28T16:36:49Z</dc:date>
    </item>
  </channel>
</rss>