<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Working condition with MPXV5100DP in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Working-condition-with-MPXV5100DP/m-p/643147#M4034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we have a system that produce both pressure and vacuum.&lt;/P&gt;&lt;P&gt;according to the spec, this sensor can measure only pressure, and its graph starts from 0kPa (although the voltage doesn't, 0kPa=0.2V).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If the sensor is under vacuum state, can it harm it?&lt;/LI&gt;&lt;LI&gt;While putting the system under vacuum state, we got a reading from the sensor, that match the vacuum level. can we use this reading and count that other sensors will give the same reading, although the sensor graph in the spec doesn't show this side of the sensor? (we want to use the range of 0-0.2V)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Eldad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:59:11 GMT</pubDate>
    <dc:creator>eldadchen</dc:creator>
    <dc:date>2026-02-03T22:59:11Z</dc:date>
    <item>
      <title>Working condition with MPXV5100DP</title>
      <link>https://community.nxp.com/t5/Sensors/Working-condition-with-MPXV5100DP/m-p/643147#M4034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we have a system that produce both pressure and vacuum.&lt;/P&gt;&lt;P&gt;according to the spec, this sensor can measure only pressure, and its graph starts from 0kPa (although the voltage doesn't, 0kPa=0.2V).&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If the sensor is under vacuum state, can it harm it?&lt;/LI&gt;&lt;LI&gt;While putting the system under vacuum state, we got a reading from the sensor, that match the vacuum level. can we use this reading and count that other sensors will give the same reading, although the sensor graph in the spec doesn't show this side of the sensor? (we want to use the range of 0-0.2V)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Eldad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Working-condition-with-MPXV5100DP/m-p/643147#M4034</guid>
      <dc:creator>eldadchen</dc:creator>
      <dc:date>2026-02-03T22:59:11Z</dc:date>
    </item>
    <item>
      <title>Re: Working condition with MPXV5100DP</title>
      <link>https://community.nxp.com/t5/Sensors/Working-condition-with-MPXV5100DP/m-p/643148#M4035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;Hi Eldad,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;The &lt;SPAN&gt;&lt;STRONG&gt;MPX5100DP&lt;/STRONG&gt;&lt;/SPAN&gt; will not be damaged as long as the pressure in port one is greater than pressure in port two (P1&amp;gt;P2). Hence if you leave P1 exposed to the atmosphere, then you can go as low in P2 as 100kPa, after that, the device would be saturated and would only provide an output of ~4.7v.&lt;BR /&gt; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: small;"&gt;Since this is a differential pressure sensor, the reading you got from the sensor will match the vacuum level so, I can confirm to you that this will work for any other &lt;SPAN&gt;&lt;STRONG&gt;MPX5100DP. &lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 21:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Working-condition-with-MPXV5100DP/m-p/643148#M4035</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-04-04T21:15:31Z</dc:date>
    </item>
  </channel>
</rss>