<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックPressure sensor selection</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626900#M3888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'd like help selection an air pressure sensor chip for a new product. I'll give a summary of our requirements here:&lt;/P&gt;&lt;P&gt;- Size: Not critical, but we're looking for a PCB-mount chip to measure the air pressure at the chip.&lt;/P&gt;&lt;P&gt;- Pressure range: Normal ambient pressures at normal ground altitudes.&lt;/P&gt;&lt;P&gt;- Operating temperature range: Preferably at least 0-60 Celsius.&lt;/P&gt;&lt;P&gt;- Interface: For design simplicity, an I2C or SPI interface would be highly desirable.&lt;/P&gt;&lt;P&gt;- Sample rate: We need accurate data at about 10Hz, so allowing for noise I expect we need about 100Hz or higher.&lt;/P&gt;&lt;P&gt;- Voltage: Preferably 3.3V, but we can probably design around 1.8V or 5V.&lt;/P&gt;&lt;P&gt;- Power: Fairly important, preferably in the Milliampere range, but we can make allowances for more power if necessary.&lt;/P&gt;&lt;P&gt;- Cost: Around a couple of dollars per chip.&lt;/P&gt;&lt;P&gt;- Accuracy: This is critical. We do not need absolute accuracy or temperature stability, but we need to accurately measure pressure differences over a period of seconds with a resolution of 1Pa (0.001 kPa). We're well aware that this will be beyond the specifications of any chip we choose, but I believe that over a period of seconds with no need for temperature stability or stability over longer periods of time, and appropriately filtering the data to remove noise, we should be able to achieve a 1Pa resolution for measuring pressure difference at about a 10Hz rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:46:56 GMT</pubDate>
    <dc:creator>jeffrickard</dc:creator>
    <dc:date>2026-02-03T22:46:56Z</dc:date>
    <item>
      <title>Pressure sensor selection</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626900#M3888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'd like help selection an air pressure sensor chip for a new product. I'll give a summary of our requirements here:&lt;/P&gt;&lt;P&gt;- Size: Not critical, but we're looking for a PCB-mount chip to measure the air pressure at the chip.&lt;/P&gt;&lt;P&gt;- Pressure range: Normal ambient pressures at normal ground altitudes.&lt;/P&gt;&lt;P&gt;- Operating temperature range: Preferably at least 0-60 Celsius.&lt;/P&gt;&lt;P&gt;- Interface: For design simplicity, an I2C or SPI interface would be highly desirable.&lt;/P&gt;&lt;P&gt;- Sample rate: We need accurate data at about 10Hz, so allowing for noise I expect we need about 100Hz or higher.&lt;/P&gt;&lt;P&gt;- Voltage: Preferably 3.3V, but we can probably design around 1.8V or 5V.&lt;/P&gt;&lt;P&gt;- Power: Fairly important, preferably in the Milliampere range, but we can make allowances for more power if necessary.&lt;/P&gt;&lt;P&gt;- Cost: Around a couple of dollars per chip.&lt;/P&gt;&lt;P&gt;- Accuracy: This is critical. We do not need absolute accuracy or temperature stability, but we need to accurately measure pressure differences over a period of seconds with a resolution of 1Pa (0.001 kPa). We're well aware that this will be beyond the specifications of any chip we choose, but I believe that over a period of seconds with no need for temperature stability or stability over longer periods of time, and appropriately filtering the data to remove noise, we should be able to achieve a 1Pa resolution for measuring pressure difference at about a 10Hz rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626900#M3888</guid>
      <dc:creator>jeffrickard</dc:creator>
      <dc:date>2026-02-03T22:46:56Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure sensor selection</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626901#M3889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP pressure sensors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Based on your requirements, I would recommend considering the &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/barometric-pressure-15-to-115-kpa/20-to-110kpa-absolute-digital-pressure-sensor:MPL3115A2"&gt;MPL3115A2&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Size: 3 x 5 x 1.25mm 8-pin LGA package&lt;/P&gt;&lt;P&gt;- Calibrated pressure range: 50kPa to 110kPa absolute pressure&lt;/P&gt;&lt;P&gt;- Operating temperature range: −40°C to +85°C&lt;/P&gt;&lt;P&gt;- Interface: I2C only&lt;/P&gt;&lt;P&gt;- Sample rate: Depending on OS[2:0] bits, more in Table 46 of &lt;A href="http://cache.nxp.com/files/sensors/doc/data_sheet/MPL3115A2.pdf"&gt;MPL3115 datasheet&lt;/A&gt;&lt;/P&gt;&lt;P&gt;- Voltage: 3.3V is OK (1.95V – 3.6V)&lt;/P&gt;&lt;P&gt;- Power: Depending on OS[2:0] bits, more in Table 6 of MPL3115 datasheet, the max current during acquisition and conversion is 2mA&lt;/P&gt;&lt;P&gt;- Cost: 1K @ US$1.69&lt;/P&gt;&lt;P&gt;- Accuracy/Resolution: Depending on OS[2:0] bits, theoretically 1.5Pa @ max OS[2:0] = 0b111, a quick test on my desk:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6347i8E681D7551C936BB/image-size/large?v=v2&amp;amp;px=999" title="pressure1.JPG" alt="pressure1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To evaluate the MPL3115A2, we can offer a complete demo kit, an Arduino/Freedom compatible shield board or just a breakout board - &lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/freedom-development-boards/sensor-toolbox-development-platform-for-mpl3115a2-pressure-altimeter-sensor:FRDMSTBC-P3115" title="http://www.nxp.com/products/software-and-tools/hardware-development-tools/freedom-development-boards/sensor-toolbox-development-platform-for-mpl3115a2-pressure-altimeter-sensor:FRDMSTBC-P3115"&gt;MPL3115A2 Pressure Sensor Development Boards|NXP.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any further questions, please let me know.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="margin: 0px; padding: 0px; border: 0px; font-weight: normal; font-style: italic; font-size: 11px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; vertical-align: baseline; color: #51626f; font-variant-ligatures: normal; font-variant-caps: normal; letter-spacing: normal; orphans: 2; text-align: left; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; line-height: 19.03px; background-color: #ffffff;"&gt;PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 10:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626901#M3889</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-09-19T10:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure sensor selection</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626902#M3890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help. I'll order a couple, attach it to our current&lt;/P&gt;&lt;P&gt;prototype, and see how it performs. Based on the datasheet it looks like&lt;/P&gt;&lt;P&gt;the accuracy may only just manage to fit our requirements - a bit faster&lt;/P&gt;&lt;P&gt;and a bit more accurate would be better - but there's a good chance that in&lt;/P&gt;&lt;P&gt;real-world conditions we'll have more problems with accuracy due to the&lt;/P&gt;&lt;P&gt;housing (porting, vibration) than due to the sensor. We'll soon find out!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On 19 September 2016 at 12:20, TomasVaverka &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 05:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-selection/m-p/626902#M3890</guid>
      <dc:creator>jeffrickard</dc:creator>
      <dc:date>2016-09-20T05:22:59Z</dc:date>
    </item>
  </channel>
</rss>