<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MPL3115A2 register INT_SOURCE</title>
    <link>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624281#M3853</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The source is the Pressure and Temperature output registers. Once the interrupt is asserted it is cleared by reading the appropriate output register. For Pressure interrupts this would be OUT_P_MSB and for Temperature interrupts it would be OUT_T_MSB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Mar 2017 17:32:34 GMT</pubDate>
    <dc:creator>miguelsalhuana</dc:creator>
    <dc:date>2017-03-06T17:32:34Z</dc:date>
    <item>
      <title>MPL3115A2 register INT_SOURCE</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624280#M3852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I’m trying to understand a little about the MPL3115A2 pressure sensor we are using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Section 13.11, INT_SOURCE (0x12), second paragraph: “The setting of the bits is rising edge sensitive, the bit is set by a low to high state change and reset by reading the appropriate source register”.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What does this mean for the SRC_PW and SRC_TW bits, i.e., what is the source? Does this mean to reading this register (INT_SOURCE) will clear these bits, or must I read another “source” register?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624280#M3852</guid>
      <dc:creator>dkh</dc:creator>
      <dc:date>2026-02-03T22:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 register INT_SOURCE</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624281#M3853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The source is the Pressure and Temperature output registers. Once the interrupt is asserted it is cleared by reading the appropriate output register. For Pressure interrupts this would be OUT_P_MSB and for Temperature interrupts it would be OUT_T_MSB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 17:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624281#M3853</guid>
      <dc:creator>miguelsalhuana</dc:creator>
      <dc:date>2017-03-06T17:32:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 register INT_SOURCE</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624282#M3854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, reading the output for the pressure clears the PTH bit as well ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 00:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624282#M3854</guid>
      <dc:creator>dkh</dc:creator>
      <dc:date>2017-03-07T00:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 register INT_SOURCE</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624283#M3855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes for the pressure interrupts reading OUT_P_MSB register will clear the interrupt. For the temperature interrupts reading OUT_T_MSB register will clear the interrupts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 00:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-register-INT-SOURCE/m-p/624283#M3855</guid>
      <dc:creator>miguelsalhuana</dc:creator>
      <dc:date>2017-03-07T00:33:19Z</dc:date>
    </item>
  </channel>
</rss>