<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMMA8451Q  interrupt read mode</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8451Q-interrupt-read-mode/m-p/614437#M3757</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I configured the MMA8451Q with ODR = 800Hz, so I can read the acceleration's components with a 1,25 ms &amp;nbsp;sample period.&lt;/P&gt;&lt;P&gt;The &amp;nbsp;polling mode is ok, I can do a read with &amp;nbsp;800Hz sample frequency.&lt;/P&gt;&lt;P&gt;But I can do it in "interrupt mode" (I configured MMA8551 as described in AN4076) because I see the interrupt pulse every 24 ms (about 40 Hz).&lt;/P&gt;&lt;P&gt;Why?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:36:26 GMT</pubDate>
    <dc:creator>maurogatti</dc:creator>
    <dc:date>2026-02-03T22:36:26Z</dc:date>
    <item>
      <title>MMA8451Q  interrupt read mode</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-interrupt-read-mode/m-p/614437#M3757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I configured the MMA8451Q with ODR = 800Hz, so I can read the acceleration's components with a 1,25 ms &amp;nbsp;sample period.&lt;/P&gt;&lt;P&gt;The &amp;nbsp;polling mode is ok, I can do a read with &amp;nbsp;800Hz sample frequency.&lt;/P&gt;&lt;P&gt;But I can do it in "interrupt mode" (I configured MMA8551 as described in AN4076) because I see the interrupt pulse every 24 ms (about 40 Hz).&lt;/P&gt;&lt;P&gt;Why?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-interrupt-read-mode/m-p/614437#M3757</guid>
      <dc:creator>maurogatti</dc:creator>
      <dc:date>2026-02-03T22:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q  interrupt read mode</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-interrupt-read-mode/m-p/614438#M3758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mauro,&lt;/P&gt;&lt;P&gt;Thank you very much for writing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, I highly recommend to use the sample project from the link below as a reference for your application:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-98836"&gt;https://community.nxp.com/docs/DOC-98836&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that in the project, the interrupt mode is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you have any further question and I will be glad to help you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 16:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-interrupt-read-mode/m-p/614438#M3758</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2016-11-25T16:55:37Z</dc:date>
    </item>
  </channel>
</rss>