<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MMA8652, problem with freefall/motion flag reading. Desperately need help!</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8652-problem-with-freefall-motion-flag-reading-Desperately/m-p/609710#M3731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try using the embedded transient detection function that triggers an interrupt when any of the enabled axes has exceeded a set acceleration threshold disregarding the static acceleration. So the data that is compared to the threshold to be exceeded is high-pass filtered data. For more info, please refer to the &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4071.pdf"&gt;AN4071&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 08:43:48 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2016-11-22T08:43:48Z</dc:date>
    <item>
      <title>MMA8652, problem with freefall/motion flag reading. Desperately need help!</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8652-problem-with-freefall-motion-flag-reading-Desperately/m-p/609709#M3730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I am using MMA8652FC accelerometer in on of my developments and desperately need help to solve the following problem as I am way behind schedule because of this.&lt;/P&gt;&lt;P&gt;Regardless of the setting of "OAE" and "ELE" in FF_MT_CFG Reg:0x15 and values in 0x017 and 0x018, bit "EA" in FF_MT_SRC 0x016 is getting locked with "Z" axis up. Entire register is acting more like Portrait/Landscape at 0x10.&lt;/P&gt;&lt;P&gt;My intentions are simply to read the motion bit in 0x16 and activate, or deactivate the light.&amp;nbsp;&lt;BR /&gt;What am I doing wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8652-problem-with-freefall-motion-flag-reading-Desperately/m-p/609709#M3730</guid>
      <dc:creator>samkuliev</dc:creator>
      <dc:date>2026-02-03T22:36:12Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8652, problem with freefall/motion flag reading. Desperately need help!</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8652-problem-with-freefall-motion-flag-reading-Desperately/m-p/609710#M3731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try using the embedded transient detection function that triggers an interrupt when any of the enabled axes has exceeded a set acceleration threshold disregarding the static acceleration. So the data that is compared to the threshold to be exceeded is high-pass filtered data. For more info, please refer to the &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4071.pdf"&gt;AN4071&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 08:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8652-problem-with-freefall-motion-flag-reading-Desperately/m-p/609710#M3731</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-11-22T08:43:48Z</dc:date>
    </item>
  </channel>
</rss>