<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: TPMS sensor</title>
    <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590577#M3579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Tomas, I will look into it. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 11:25:55 GMT</pubDate>
    <dc:creator>balajykumar</dc:creator>
    <dc:date>2016-08-11T11:25:55Z</dc:date>
    <item>
      <title>TPMS sensor</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590573#M3575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in a design phase of TPMS Board. I have chosen this part FXTH8715116T1 but it can support only minimum pressure sensing range of 100kpa ( ie 14.5 psi). I need min 4 psi ( ie.27.5 kpa) for my application . kindly suggest any external sensor which can support that range and also integrate with that part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590573#M3575</guid>
      <dc:creator>balajykumar</dc:creator>
      <dc:date>2026-02-03T22:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS sensor</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590574#M3576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Balajy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend the &lt;A href="http://www.nxp.com/files/sensors/doc/data_sheet/MP3H6115A.pdf"&gt;MP3H6115A&lt;/A&gt; which is an integrated 3V analog absolute pressure sensor operating in the range of 15kPa to 115kPa. It has temperature compensation, calibration and amplifier circuitry on–chip and its output voltage for full rated pressure is typically 2.82V. You can connect its output (pin #4) to either PTA0 (AD3) or PTA1 (AD4) pins of the FXTH8715116T1 and use the corresponding routines (TPMS_READ_V0 or TPMS_READ_V1) to read the output voltage of the MP3H6115A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-weight: normal; font-style: italic; font-size: 11px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f; text-align: left; text-indent: 0px;"&gt;&lt;EM&gt;PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 09:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590574#M3576</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-08-11T09:01:39Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS sensor</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590575#M3577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I forgot to add my maximum requirement in the previous conversation. My input requirement range is 4 to 45 psi.But the above part can support&amp;nbsp; max 16.5psi only. can you please suggest any other part which can support the above requirement?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whether this sensor can meet the software compatibility with FXTH8715116T1? kindly provide your suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 09:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590575#M3577</guid>
      <dc:creator>balajykumar</dc:creator>
      <dc:date>2016-08-11T09:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS sensor</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590576#M3578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Balajy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only absolute pressure sensor supporting 45psi is the &lt;A href="http://cache.nxp.com/files/sensors/doc/data_sheet/MPXH6400A.pdf"&gt;MPXH6400A&lt;/A&gt;. It is trimmed at 5V, but works well at 3V. You can order free samples from &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/lpg-and-cng-gas-15-to-400-kpa/absolute-integrated-pressure-sensor-15-to-400kpa:MPXx6400?&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab"&gt;this&lt;/A&gt; website and test it in your application whether it meets your requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 10:58:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590576#M3578</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-08-11T10:58:11Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS sensor</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590577#M3579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Tomas, I will look into it. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 11:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-sensor/m-p/590577#M3579</guid>
      <dc:creator>balajykumar</dc:creator>
      <dc:date>2016-08-11T11:25:55Z</dc:date>
    </item>
  </channel>
</rss>