<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MPL115A2 temperature measurement?</title>
    <link>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167585#M35</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know this post is from last year.&lt;/P&gt;&lt;P&gt;But I have the same problem.&lt;/P&gt;&lt;P&gt;According to the Datasheet the Temperature-ADC-Value is 472 at 25°C. While each degree counts -5.35.&lt;/P&gt;&lt;P&gt;So if I use " Temp = (ADC_val - 472)/-5.35 +25"&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got "11" at 21°C. So if I use "Temp = (ADC_val - 472)/-5.35 +35 "﻿ I got the right value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I think theres a mistake in the Datasheet (and Application Note AN3785 too). Because "472" @25°C can't be right. I have something about 520-530&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Aug 2011 19:18:19 GMT</pubDate>
    <dc:creator>MasterFX</dc:creator>
    <dc:date>2011-08-30T19:18:19Z</dc:date>
    <item>
      <title>MPL115A2 temperature measurement?</title>
      <link>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167584#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Hi Guys,&lt;BR /&gt;Does anybody know if it is possible to get accurate temperature form data delivered by the sensor. I tried to use following equation:&lt;BR /&gt;&lt;BR /&gt;Temp_comp = (605.75 - Temp_ADC) / 5.35&lt;BR /&gt;&lt;BR /&gt;but calculated temperature was smaller than it should be. Any ideas? Best regards... Robert&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167584#M34</guid>
      <dc:creator>robekw</dc:creator>
      <dc:date>2026-02-03T22:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPL115A2 temperature measurement?</title>
      <link>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167585#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know this post is from last year.&lt;/P&gt;&lt;P&gt;But I have the same problem.&lt;/P&gt;&lt;P&gt;According to the Datasheet the Temperature-ADC-Value is 472 at 25°C. While each degree counts -5.35.&lt;/P&gt;&lt;P&gt;So if I use " Temp = (ADC_val - 472)/-5.35 +25"&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got "11" at 21°C. So if I use "Temp = (ADC_val - 472)/-5.35 +35 "﻿ I got the right value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I think theres a mistake in the Datasheet (and Application Note AN3785 too). Because "472" @25°C can't be right. I have something about 520-530&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2011 19:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167585#M35</guid>
      <dc:creator>MasterFX</dc:creator>
      <dc:date>2011-08-30T19:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: MPL115A2 temperature measurement?</title>
      <link>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167586#M36</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same problem of figuring out how to convert Tadc to actual degrees.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the response from Freescale:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Anyway, while we output temp on MPL115A, the temp sensor is used to calibrate and make our Pressure output more accurate, not provide accurate temperature determination. That was a cost reduction choice. If we provided a calibrated temperature, then we would add cost to the test procedure. The next generation MPL3115A now has calibrated temp output. Its production is is end of Q4 this year.﻿&lt;/P&gt;&lt;P class="MsoPlainText"&gt;Regarding temperature conversion, the fact is that the 25 deg C is supposed to be set at 472 ADC counts on the Tadc output from MPL115A. It is a negative slope, such that its -5.35 ADC counts per a deg C. I worked out the transfer function to be somewhat like:&lt;/P&gt;&lt;P class="MsoPlainText"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText"&gt;Temp = (Tadc - 605.75) / -5.35&lt;/P&gt;&lt;P class="MsoPlainText"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoPlainText"&gt;At -40 deg C the output value should be of 819.75 and at 105 deg C the output value should be of 44.&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoPlainText"&gt;Note that because the value is a 10 bit, it cannot in the real world always be assumed to be a full range output. Even a 9 bit number cannot accommodate this range, so its 10.&lt;SPAN&gt;&amp;nbsp;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText"&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 20:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167586#M36</guid>
      <dc:creator>bmedic</dc:creator>
      <dc:date>2011-09-02T20:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: MPL115A2 temperature measurement?</title>
      <link>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167587#M37</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok this helps a little bit, but it does not explain why the adc-count at 25°C is 530 instead of 472. So the temperature differs about 10 degree. Isn't this a too big variance, even for a uncalibrated temperature-sensor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Sep 2011 20:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL115A2-temperature-measurement/m-p/167587#M37</guid>
      <dc:creator>MasterFX</dc:creator>
      <dc:date>2011-09-03T20:59:28Z</dc:date>
    </item>
  </channel>
</rss>