<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックGaming Handset</title>
    <link>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/548252#M3380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using FRDM-K64F and FRDM-FXS-MULT2-B to test the new sensor fusion library V 7.00.&lt;/P&gt;&lt;P&gt;I downloaded KSDK2.0 for FRDM-K64F and compile the sample code under "baremetal_mult2b" for sensor fusion.&lt;/P&gt;&lt;P&gt;I downloaded the executable code to FRDM-K64F and works fine.&lt;/P&gt;&lt;P&gt;When I am trying the gaming handset mode, the heading is keeping the change(0.2 degree per s) and it is almost the same as fusion V5.00 when it is stationary because of gyro drifting.&lt;/P&gt;&lt;P&gt;I was told that you added the new function to avoid this in V7.00 and I am going to try it.&lt;/P&gt;&lt;P&gt;Could you tell me if I need to set some threshold to avoid drifting when in stationary?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:05:56 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2026-02-03T21:05:56Z</dc:date>
    <item>
      <title>Gaming Handset</title>
      <link>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/548252#M3380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using FRDM-K64F and FRDM-FXS-MULT2-B to test the new sensor fusion library V 7.00.&lt;/P&gt;&lt;P&gt;I downloaded KSDK2.0 for FRDM-K64F and compile the sample code under "baremetal_mult2b" for sensor fusion.&lt;/P&gt;&lt;P&gt;I downloaded the executable code to FRDM-K64F and works fine.&lt;/P&gt;&lt;P&gt;When I am trying the gaming handset mode, the heading is keeping the change(0.2 degree per s) and it is almost the same as fusion V5.00 when it is stationary because of gyro drifting.&lt;/P&gt;&lt;P&gt;I was told that you added the new function to avoid this in V7.00 and I am going to try it.&lt;/P&gt;&lt;P&gt;Could you tell me if I need to set some threshold to avoid drifting when in stationary?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/548252#M3380</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2026-02-03T21:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: Gaming Handset</title>
      <link>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/548253#M3381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Christie,&lt;/P&gt;&lt;P&gt;That feature is not part of the default build, but is easy to add.&amp;nbsp; It essentially just shuts down the fusion operation when the board is stationary.&amp;nbsp; I'll upload an alternate main() for you to use in another post momentarily.&amp;nbsp; See Section 4.8, Fusion Standby mode, in the user guide for a detailed discussion.&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 18:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/548253#M3381</guid>
      <dc:creator>michaelestanley</dc:creator>
      <dc:date>2016-08-22T18:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: Gaming Handset</title>
      <link>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/2013474#M8609</link>
      <description>&lt;P&gt;Gaming handsets are taking innovation to the next level! Recently, I discovered an option to explore a specialized &lt;A href="https://bons.pro.in/app/" target="_self"&gt;app download&lt;/A&gt; for enhancing gaming experiences. These apps focus on providing seamless performance, which is ideal for both casual and competitive gamers. A great way to improve mobile gaming capabilities!&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 08:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Gaming-Handset/m-p/2013474#M8609</guid>
      <dc:creator>Ritayougs</dc:creator>
      <dc:date>2024-12-13T08:54:36Z</dc:date>
    </item>
  </channel>
</rss>