<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re:  FRDM-STBC-AGM01 voltage</title>
    <link>https://community.nxp.com/t5/Sensors/FRDM-STBC-AGM01-voltage/m-p/540894#M3367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I²C pin (SDA and SCL)&amp;nbsp; are usually "open drain", and pull up resistors are required to make the communication works. So you would be able to drive the board with 2 pull up resistors connected to 3.3V.&lt;/P&gt;&lt;P&gt;Please check out the following webpage: &lt;A href="http://playground.arduino.cc/Main/I2CBi-directionalLevelShifter" title="http://playground.arduino.cc/Main/I2CBi-directionalLevelShifter"&gt;Arduino Playground - I2CBi-directionalLevelShifter&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Aug 2016 07:51:55 GMT</pubDate>
    <dc:creator>anthonyduhamel</dc:creator>
    <dc:date>2016-08-22T07:51:55Z</dc:date>
    <item>
      <title>FRDM-STBC-AGM01 voltage</title>
      <link>https://community.nxp.com/t5/Sensors/FRDM-STBC-AGM01-voltage/m-p/540893#M3366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I managed to get the board working but there is one thing that bothers me. Arduino is a 5V device but max VDD for FXAS21002C and FXOS8700CQ is 3.3V. So the SDA and SCL (or SCLK and MOSI) coming from arduino is 5V. I read the datasheet but there is no info about 5V tolarance. Can it damage in any way FXAS21002C or FXOS8700CQ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FRDM-STBC-AGM01-voltage/m-p/540893#M3366</guid>
      <dc:creator>def152</dc:creator>
      <dc:date>2026-02-03T22:53:07Z</dc:date>
    </item>
    <item>
      <title>Re:  FRDM-STBC-AGM01 voltage</title>
      <link>https://community.nxp.com/t5/Sensors/FRDM-STBC-AGM01-voltage/m-p/540894#M3367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I²C pin (SDA and SCL)&amp;nbsp; are usually "open drain", and pull up resistors are required to make the communication works. So you would be able to drive the board with 2 pull up resistors connected to 3.3V.&lt;/P&gt;&lt;P&gt;Please check out the following webpage: &lt;A href="http://playground.arduino.cc/Main/I2CBi-directionalLevelShifter" title="http://playground.arduino.cc/Main/I2CBi-directionalLevelShifter"&gt;Arduino Playground - I2CBi-directionalLevelShifter&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 07:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FRDM-STBC-AGM01-voltage/m-p/540894#M3367</guid>
      <dc:creator>anthonyduhamel</dc:creator>
      <dc:date>2016-08-22T07:51:55Z</dc:date>
    </item>
  </channel>
</rss>