<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K22 Freedom board with intelligent Sensing Framework v2.0 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/K22-Freedom-board-with-intelligent-Sensing-Framework-v2-0/m-p/506656#M3160</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the K22 Freedom board with the FRDM-STBC-AGM01. Everthing seems to work great. I am also using the Intelligent Sensing Framework v2.0 and following along with the&amp;nbsp; the traning videos. I discovered the "Kinetis Interface Tool" watching the 3rd video. So I downloaded it and tried to use it. However it will not reconize the board(s). The correct com port number shows up but I get a "No Compatible Device found at selected COM Port!" message. Is this hardware not supported?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, when is ISF 2.2 going to be released?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:55:53 GMT</pubDate>
    <dc:creator>marks</dc:creator>
    <dc:date>2026-02-03T22:55:53Z</dc:date>
    <item>
      <title>K22 Freedom board with intelligent Sensing Framework v2.0</title>
      <link>https://community.nxp.com/t5/Sensors/K22-Freedom-board-with-intelligent-Sensing-Framework-v2-0/m-p/506656#M3160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the K22 Freedom board with the FRDM-STBC-AGM01. Everthing seems to work great. I am also using the Intelligent Sensing Framework v2.0 and following along with the&amp;nbsp; the traning videos. I discovered the "Kinetis Interface Tool" watching the 3rd video. So I downloaded it and tried to use it. However it will not reconize the board(s). The correct com port number shows up but I get a "No Compatible Device found at selected COM Port!" message. Is this hardware not supported?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, when is ISF 2.2 going to be released?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/K22-Freedom-board-with-intelligent-Sensing-Framework-v2-0/m-p/506656#M3160</guid>
      <dc:creator>marks</dc:creator>
      <dc:date>2026-02-03T22:55:53Z</dc:date>
    </item>
  </channel>
</rss>