<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pressure sensor compensation in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-compensation/m-p/150209#M31</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All the information we provide is only guaranteed under the specified conditions (0 to 85°C). Unfortunately we have no documentation regarding the MPX2010 response in the range you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This device has a differential output; therefore you’d need an instrumental amplifier. What I can suggest you is to test both, the sensor and your amplifier in the -40° to 40°C, so you can characterize the full system response. Your amplifiers gain factor would change as well as the sensors behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPX2010 is a linear device but the temperature factor would change from one range to another, i.e. the transfer function would not be the same at -40°C than at -10°C. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you have the system response in the full range (you already have from 0 to 40°C) you can generate a transfer function to obtain the pressure value. I’d also recommend you to use a microcontroller with an integrated temperature sensor, so you can change your temperature factor as needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps. =)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Oct 2012 15:41:29 GMT</pubDate>
    <dc:creator>Joshevelle</dc:creator>
    <dc:date>2012-10-05T15:41:29Z</dc:date>
    <item>
      <title>Pressure sensor compensation</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-compensation/m-p/150208#M30</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have to use the mpxm2010 sensor in a -40 to +40 tem range. This sensor is compensated in the 0 to +85 range. With a temperature sensor, how can i do to correct the drift in negative temperature range? What is the formula to correct the pressure value ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-compensation/m-p/150208#M30</guid>
      <dc:creator>Beta</dc:creator>
      <dc:date>2026-02-03T23:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure sensor compensation</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-sensor-compensation/m-p/150209#M31</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All the information we provide is only guaranteed under the specified conditions (0 to 85°C). Unfortunately we have no documentation regarding the MPX2010 response in the range you need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This device has a differential output; therefore you’d need an instrumental amplifier. What I can suggest you is to test both, the sensor and your amplifier in the -40° to 40°C, so you can characterize the full system response. Your amplifiers gain factor would change as well as the sensors behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPX2010 is a linear device but the temperature factor would change from one range to another, i.e. the transfer function would not be the same at -40°C than at -10°C. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you have the system response in the full range (you already have from 0 to 40°C) you can generate a transfer function to obtain the pressure value. I’d also recommend you to use a microcontroller with an integrated temperature sensor, so you can change your temperature factor as needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps. =)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Oct 2012 15:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-sensor-compensation/m-p/150209#M31</guid>
      <dc:creator>Joshevelle</dc:creator>
      <dc:date>2012-10-05T15:41:29Z</dc:date>
    </item>
  </channel>
</rss>