<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPR121 SET / CLEAR register bytes problems in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPR121-SET-CLEAR-register-bytes-problems/m-p/497384#M3097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I bought a MPR121 breakout sensor. I have set the 4 touch sensors an 8 LEDs Outs on GPIO 4 to 11. GPIO 4 is bit b0 and GPIO 11 is b7, All works fine, I sent 0x0F to SET register (0x78) and 0xF0 to Clear Register (0x79) and I can see the proper leds ON and OFF (ELE4/LED0 to ELE7/LED3 high). But when I sent a 0x20 (0010000b) to SET register and 0xBF (11011111b) to the Clear register, I saw ELE/10LED6 HIGH (like 01000000b). By Other hand when I sent the values for 01000000b, I saw 00100000b. I have checked the wires a lot of times. It looks like LED 6 and LED 5 are changed from the DATA register to the real pin...Do you have any errata data sheet? Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:03:30 GMT</pubDate>
    <dc:creator>joseluiscaresan</dc:creator>
    <dc:date>2026-02-03T23:03:30Z</dc:date>
    <item>
      <title>MPR121 SET / CLEAR register bytes problems</title>
      <link>https://community.nxp.com/t5/Sensors/MPR121-SET-CLEAR-register-bytes-problems/m-p/497384#M3097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I bought a MPR121 breakout sensor. I have set the 4 touch sensors an 8 LEDs Outs on GPIO 4 to 11. GPIO 4 is bit b0 and GPIO 11 is b7, All works fine, I sent 0x0F to SET register (0x78) and 0xF0 to Clear Register (0x79) and I can see the proper leds ON and OFF (ELE4/LED0 to ELE7/LED3 high). But when I sent a 0x20 (0010000b) to SET register and 0xBF (11011111b) to the Clear register, I saw ELE/10LED6 HIGH (like 01000000b). By Other hand when I sent the values for 01000000b, I saw 00100000b. I have checked the wires a lot of times. It looks like LED 6 and LED 5 are changed from the DATA register to the real pin...Do you have any errata data sheet? Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR121-SET-CLEAR-register-bytes-problems/m-p/497384#M3097</guid>
      <dc:creator>joseluiscaresan</dc:creator>
      <dc:date>2026-02-03T23:03:30Z</dc:date>
    </item>
  </channel>
</rss>