<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Sensor MPL3115A2</title>
    <link>https://community.nxp.com/t5/Sensors/Sensor-MPL3115A2/m-p/494015#M3050</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, I would not recommend to solder the MPL3115A2 in the vapor phase oven without sticking the hole in the sensor cover because high humid and heat media have the potential to dissolve, or be absorbed by the gel and corrupt the die surface or lead to wire-bond breakage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, sealing the hole on the sensor with kapton tape is absolutely recommended.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Jose&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Feb 2016 15:19:43 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2016-02-08T15:19:43Z</dc:date>
    <item>
      <title>Sensor MPL3115A2</title>
      <link>https://community.nxp.com/t5/Sensors/Sensor-MPL3115A2/m-p/494014#M3049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sensor MPL3115A2 - Is it possible to solder this sensor in the vapor phase oven without sticking the hole in the sensors cover?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Sensor-MPL3115A2/m-p/494014#M3049</guid>
      <dc:creator>monikafuchsova</dc:creator>
      <dc:date>2026-02-03T23:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: Sensor MPL3115A2</title>
      <link>https://community.nxp.com/t5/Sensors/Sensor-MPL3115A2/m-p/494015#M3050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, I would not recommend to solder the MPL3115A2 in the vapor phase oven without sticking the hole in the sensor cover because high humid and heat media have the potential to dissolve, or be absorbed by the gel and corrupt the die surface or lead to wire-bond breakage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, sealing the hole on the sensor with kapton tape is absolutely recommended.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Jose&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 15:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Sensor-MPL3115A2/m-p/494015#M3050</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2016-02-08T15:19:43Z</dc:date>
    </item>
  </channel>
</rss>