<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Expectations to MPR121</title>
    <link>https://community.nxp.com/t5/Sensors/Expectations-to-MPR121/m-p/238995#M294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp; I have had success using the MPR121 with 5x5mm copper buttons and 2mm overlay.&amp;nbsp; I also found the proximity detection feature to be helpful as it ties the buttons together into one net.&amp;nbsp; For an array of 12 small 5x5mm buttons I found that this could detect a hand approaching at about 2cm.&amp;nbsp; Overall the device is not extremely sensitive but is effective for small buttons with non-conductive overlays.&amp;nbsp; I have not tried an OLED display, but my guess is that the buttons would not work through the display, maybe try ITO on a clear film on top of the OLED display with "traces" in the shape of buttons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Aug 2013 17:22:04 GMT</pubDate>
    <dc:creator>bryce</dc:creator>
    <dc:date>2013-08-08T17:22:04Z</dc:date>
    <item>
      <title>Expectations to MPR121</title>
      <link>https://community.nxp.com/t5/Sensors/Expectations-to-MPR121/m-p/238994#M293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i've played around with a MPR121 Touch Sensor. I'm not sure what i can expect from the touch sensor, so i would ask other community members about their experiences with the sensor. What is the biggest distance from a sensor field and a finger to recognize a "touch". Is it possible to mount an OLED display in front of the sensor field?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2013 07:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Expectations-to-MPR121/m-p/238994#M293</guid>
      <dc:creator>mariod</dc:creator>
      <dc:date>2013-03-25T07:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: Expectations to MPR121</title>
      <link>https://community.nxp.com/t5/Sensors/Expectations-to-MPR121/m-p/238995#M294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp; I have had success using the MPR121 with 5x5mm copper buttons and 2mm overlay.&amp;nbsp; I also found the proximity detection feature to be helpful as it ties the buttons together into one net.&amp;nbsp; For an array of 12 small 5x5mm buttons I found that this could detect a hand approaching at about 2cm.&amp;nbsp; Overall the device is not extremely sensitive but is effective for small buttons with non-conductive overlays.&amp;nbsp; I have not tried an OLED display, but my guess is that the buttons would not work through the display, maybe try ITO on a clear film on top of the OLED display with "traces" in the shape of buttons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 17:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Expectations-to-MPR121/m-p/238995#M294</guid>
      <dc:creator>bryce</dc:creator>
      <dc:date>2013-08-08T17:22:04Z</dc:date>
    </item>
  </channel>
</rss>