<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックPressure Sensor MPX5700ASX</title>
    <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480492#M2804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! We use the Pressure Sensor MPX5700ASX. Could you explaine: is it normally or defect of sensor when we have a leak of air from a back hole?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:35:17 GMT</pubDate>
    <dc:creator>ulbin</dc:creator>
    <dc:date>2026-02-03T22:35:17Z</dc:date>
    <item>
      <title>Pressure Sensor MPX5700ASX</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480492#M2804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! We use the Pressure Sensor MPX5700ASX. Could you explaine: is it normally or defect of sensor when we have a leak of air from a back hole?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480492#M2804</guid>
      <dc:creator>ulbin</dc:creator>
      <dc:date>2026-02-03T22:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPX5700ASX</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480493#M2805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, it is not normal to have a leak of air in the back hole of the device. This can only means that the internal gel/diaphragm is damaged.&lt;/P&gt;&lt;P&gt;This kind of issue is typically caused due to an excessive pressure applied to the sensor, a negative pressure (vacuum) was applied to the sensor, temperatures below/above the specified in the datasheet or because it has being used to measure pressure in a different media than “Dry clean air”. If none of this is true for your case, then it is probable that the pressure sensor is defective.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 15:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480493#M2805</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2016-04-05T15:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPX5700ASX</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480494#M2806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! Thanks for your reply. But we have one more question: could it cause damage of sensor when there was a sharp pressure relief of compressed air with the capacity of 60 litres from 500 kPa to zero?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 09:12:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480494#M2806</guid>
      <dc:creator>ulbin</dc:creator>
      <dc:date>2016-04-06T09:12:54Z</dc:date>
    </item>
    <item>
      <title>Re: Pressure Sensor MPX5700ASX</title>
      <link>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480495#M2807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That should not be a problem as long as in the sharp pressure relief, the pressure never goes below to zero (negative pressure/vacuum).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 20:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Pressure-Sensor-MPX5700ASX/m-p/480495#M2807</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2016-04-06T20:09:45Z</dc:date>
    </item>
  </channel>
</rss>