<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mpl115a1 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/mpl115a1/m-p/463437#M2607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPL115A1 remains active as it is the only SPI output pressure sensor currently available in our portfolio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPL115A2 is not recommended for new designs as there is a newer part – &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/barometric-pressure-15-to-115-kpa/20-to-110kpa-absolute-digital-pressure-sensor:MPL3115A2"&gt;MPL3115A2&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31565i400853E55542FC93/image-size/large?v=v2&amp;amp;px=999" title="MPL115A.JPG" alt="MPL115A.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jan 2016 14:19:02 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2016-01-04T14:19:02Z</dc:date>
    <item>
      <title>mpl115a1</title>
      <link>https://community.nxp.com/t5/Sensors/mpl115a1/m-p/463436#M2606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;9 months ago I was told mpl115a1 was EoL and no plans for replacement. This is not shown on site is it confusion between brother part with I2C xxxA2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/mpl115a1/m-p/463436#M2606</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2026-02-03T22:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: mpl115a1</title>
      <link>https://community.nxp.com/t5/Sensors/mpl115a1/m-p/463437#M2607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPL115A1 remains active as it is the only SPI output pressure sensor currently available in our portfolio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPL115A2 is not recommended for new designs as there is a newer part – &lt;A href="http://www.nxp.com/products/sensors/pressure-sensors/barometric-pressure-15-to-115-kpa/20-to-110kpa-absolute-digital-pressure-sensor:MPL3115A2"&gt;MPL3115A2&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31565i400853E55542FC93/image-size/large?v=v2&amp;amp;px=999" title="MPL115A.JPG" alt="MPL115A.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 14:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/mpl115a1/m-p/463437#M2607</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-01-04T14:19:02Z</dc:date>
    </item>
  </channel>
</rss>