<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MAG3110 + GPS</title>
    <link>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459012#M2488</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the antenna is aluminium then you should be OK.&lt;/P&gt;&lt;P&gt;If the antenna has any iron or nickel component and is un-magnetized then the distortion will be "soft iron" in which the geomagnetic field is steered through the antenna to some extent.&lt;/P&gt;&lt;P&gt;And if the antenna has iron or nickel and is magnetized then the interference is "hard iron".&lt;/P&gt;&lt;P&gt;The Freescale magnetic calibration algorithms at &lt;A href="http://www.freescale.com/sensorfusion"&gt;www.freescale.com/sensorfusion&lt;/A&gt; should be able to correct both hard and soft iron effects. We did some successful work with an Android tablet where a ferromagnetic film behind the LCD gave a 10:1 soft iron distortion.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Nov 2015 16:04:56 GMT</pubDate>
    <dc:creator>markpedley</dc:creator>
    <dc:date>2015-11-07T16:04:56Z</dc:date>
    <item>
      <title>MAG3110 + GPS</title>
      <link>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459010#M2486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I plan to use a MAG3110 and a GPS for my application device. Does the antenna of the GPS generate too strong hard-iron interference to MAG3110 so that I can't put the two in a single PCB?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459010#M2486</guid>
      <dc:creator>suqianjin</dc:creator>
      <dc:date>2026-02-03T22:47:27Z</dc:date>
    </item>
    <item>
      <title>Re: MAG3110 + GPS</title>
      <link>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459011#M2487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suqian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's a good question. Depends if your antenna is magnetic or not... By the way, hard-iron interference is not critical if it does not exceed the MAG3110 magnetic range (+-1000uT). In any case you will have Hard-iron (the antenna will probably increase it). I understand you plan to make the MAG3110 an electronic compass right? If it is the case,&amp;nbsp; to calculate an azimut /angle you need&amp;nbsp; to calibrate the sensor to remove hard-iron bias.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your antenna may add soft-iron disruption and could bring important heading error.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26095iF72A2B37546C570A/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you to check that by taking measurements with the antenna fixed near the magnetometer. You can use a Freedom board + Sensor shield to do these measurements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2015 09:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459011#M2487</guid>
      <dc:creator>anthonyduhamel</dc:creator>
      <dc:date>2015-11-06T09:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: MAG3110 + GPS</title>
      <link>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459012#M2488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the antenna is aluminium then you should be OK.&lt;/P&gt;&lt;P&gt;If the antenna has any iron or nickel component and is un-magnetized then the distortion will be "soft iron" in which the geomagnetic field is steered through the antenna to some extent.&lt;/P&gt;&lt;P&gt;And if the antenna has iron or nickel and is magnetized then the interference is "hard iron".&lt;/P&gt;&lt;P&gt;The Freescale magnetic calibration algorithms at &lt;A href="http://www.freescale.com/sensorfusion"&gt;www.freescale.com/sensorfusion&lt;/A&gt; should be able to correct both hard and soft iron effects. We did some successful work with an Android tablet where a ferromagnetic film behind the LCD gave a 10:1 soft iron distortion.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Nov 2015 16:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MAG3110-GPS/m-p/459012#M2488</guid>
      <dc:creator>markpedley</dc:creator>
      <dc:date>2015-11-07T16:04:56Z</dc:date>
    </item>
  </channel>
</rss>