<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: Problems using two MMA8452Q simultaneously</title>
    <link>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456911#M2471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Clóvis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our last communication, the problem seems to be corrected by adding a call delay (100), correct?&lt;/P&gt;&lt;P&gt;Can you please confirm is this solved the problem?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 May 2015 17:28:25 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2015-05-25T17:28:25Z</dc:date>
    <item>
      <title>Problems using two MMA8452Q simultaneously</title>
      <link>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456910#M2470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´m trying to use two MMA8452Q simultaneously to check differents accelerations over the same body, and detect deformations while on movement. For this project I´m using an ARDUINO board for prototipation and after some succesful preliminary tests, after preparing a kit for a second phase tests the systems stop working. I already checked all the connections between and tested both accelerometers and everything is ok, but when I try to init the second accelerometer, no matter which one was the first, I got an error. The WHO_AM_I command for the second accelerometer is returning 0x01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, and sorry for english mistakes on the text above,&lt;/P&gt;&lt;P&gt;Clóvis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456910#M2470</guid>
      <dc:creator>clovismarcondes</dc:creator>
      <dc:date>2026-02-03T22:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using two MMA8452Q simultaneously</title>
      <link>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456911#M2471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Clóvis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our last communication, the problem seems to be corrected by adding a call delay (100), correct?&lt;/P&gt;&lt;P&gt;Can you please confirm is this solved the problem?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2015 17:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456911#M2471</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-05-25T17:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using two MMA8452Q simultaneously</title>
      <link>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456912#M2472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reyes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right. I´ve tried to put the delay as a workaround for the problem and it has worked. I´m not sure about the cause but I tried this to avoid possible data overrun. I have to put a minimum delay (10ms) between consecutive reads to avoid similar problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 11:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Problems-using-two-MMA8452Q-simultaneously/m-p/456912#M2472</guid>
      <dc:creator>clovismarcondes</dc:creator>
      <dc:date>2015-05-26T11:25:19Z</dc:date>
    </item>
  </channel>
</rss>