<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Import project from Code Warrior to Kinetis Design Studio in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450615#M2387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my situation. I have example project eCompass_Project. I want to edit it and try to compile it. But I have only trial version of Code Warrior. The compilation stops because of code size limitation. So I've desided to compile this project in Kinetis Design Studio.&lt;BR /&gt;I downloaded that IDE, installed and imported project via Import-&amp;gt;General-&amp;gt;Existing project into Workspace.&lt;BR /&gt; I tried to compile that but I had error:&lt;BR /&gt;&lt;STRONG style="font-size: 10pt;"&gt;Program "make" not found in PATH&lt;/STRONG&gt;&lt;BR /&gt;When I looked into the settings and I saw some troubles (see in attached files).&lt;BR /&gt;For example:&lt;BR /&gt;&lt;STRONG&gt;Orphaned configuration. No base extension cfg exists for com.freescale.coldfire.toolchain.configuration.314784377&lt;/STRONG&gt;&lt;BR /&gt;And others...&lt;/P&gt;&lt;P&gt;Hera is log of compilation:&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;make clean &lt;/P&gt;&lt;P&gt;Cannot run program "make": Launching failed&lt;/P&gt;&lt;P&gt;Error: Program "make" not found in PATH&lt;/P&gt;&lt;P&gt;PATH=[C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin/client;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/lib/i386;C:\ProgramData\Oracle\Java\javapath;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Skype\Phone\;C:\Program Files\OpenVPN\bin;C:\Freescale\KDS_3.0.0\eclipse;]&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;19:05:07 Build Finished (took 45ms)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****&amp;nbsp; of configuration FXLC95000_Internal_Flash for project eCompass_Project ****&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nothing to build for project eCompass_Project&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------------------&lt;BR /&gt;So my questions are:&lt;BR /&gt;1. Is it possible to import Code Warrior project into Kinetis Design Studio?&lt;BR /&gt;2. If it is possible, how can I do that? Can anyone give me step by step instructions? (I work with Eclipse not so long, so I don't understand some things).&lt;/P&gt;&lt;P&gt;3. Is it possible to develop software in KDS using ISF1?&lt;/P&gt;&lt;P&gt;Project consists of:&lt;/P&gt;&lt;P&gt;ISF1, FXLC95000, MAG3110, MPL3115, FXAS21002&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:40:49 GMT</pubDate>
    <dc:creator>vitaliysiplichu</dc:creator>
    <dc:date>2026-02-03T23:40:49Z</dc:date>
    <item>
      <title>Import project from Code Warrior to Kinetis Design Studio</title>
      <link>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450615#M2387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is my situation. I have example project eCompass_Project. I want to edit it and try to compile it. But I have only trial version of Code Warrior. The compilation stops because of code size limitation. So I've desided to compile this project in Kinetis Design Studio.&lt;BR /&gt;I downloaded that IDE, installed and imported project via Import-&amp;gt;General-&amp;gt;Existing project into Workspace.&lt;BR /&gt; I tried to compile that but I had error:&lt;BR /&gt;&lt;STRONG style="font-size: 10pt;"&gt;Program "make" not found in PATH&lt;/STRONG&gt;&lt;BR /&gt;When I looked into the settings and I saw some troubles (see in attached files).&lt;BR /&gt;For example:&lt;BR /&gt;&lt;STRONG&gt;Orphaned configuration. No base extension cfg exists for com.freescale.coldfire.toolchain.configuration.314784377&lt;/STRONG&gt;&lt;BR /&gt;And others...&lt;/P&gt;&lt;P&gt;Hera is log of compilation:&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;make clean &lt;/P&gt;&lt;P&gt;Cannot run program "make": Launching failed&lt;/P&gt;&lt;P&gt;Error: Program "make" not found in PATH&lt;/P&gt;&lt;P&gt;PATH=[C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin/client;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/lib/i386;C:\ProgramData\Oracle\Java\javapath;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Skype\Phone\;C:\Program Files\OpenVPN\bin;C:\Freescale\KDS_3.0.0\eclipse;]&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;19:05:07 Build Finished (took 45ms)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;****&amp;nbsp; of configuration FXLC95000_Internal_Flash for project eCompass_Project ****&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nothing to build for project eCompass_Project&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------------------&lt;BR /&gt;So my questions are:&lt;BR /&gt;1. Is it possible to import Code Warrior project into Kinetis Design Studio?&lt;BR /&gt;2. If it is possible, how can I do that? Can anyone give me step by step instructions? (I work with Eclipse not so long, so I don't understand some things).&lt;/P&gt;&lt;P&gt;3. Is it possible to develop software in KDS using ISF1?&lt;/P&gt;&lt;P&gt;Project consists of:&lt;/P&gt;&lt;P&gt;ISF1, FXLC95000, MAG3110, MPL3115, FXAS21002&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450615#M2387</guid>
      <dc:creator>vitaliysiplichu</dc:creator>
      <dc:date>2026-02-03T23:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: Import project from Code Warrior to Kinetis Design Studio</title>
      <link>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450616#M2388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #993366;"&gt;KDS supports Kinetis MCUs&amp;nbsp; only.&amp;nbsp; It does not support the FXLC95000.&amp;nbsp;&amp;nbsp; For this reason,&amp;nbsp; ISF1.1 for FXLC95000 only provides CodeWarrior projects.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 18:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450616#M2388</guid>
      <dc:creator>margaretnadworn</dc:creator>
      <dc:date>2015-05-20T18:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: Import project from Code Warrior to Kinetis Design Studio</title>
      <link>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450617#M2389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Margaret,&lt;/P&gt;&lt;P&gt;Regarding to your message if I want to develop project with FXLC95000 as hub using any ISF my only way is to buy &lt;SPAN style="color: #993366; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;CodeWarrior&lt;/SPAN&gt; license for at least $395 per year (limitation of 512K)?&lt;/P&gt;&lt;P&gt;Is where another way to use ISF example project with output file &amp;gt; 128K?&lt;/P&gt;&lt;P&gt;Maybe I can use ISF2 &lt;SPAN style="color: #993366; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;for FXLC95000&lt;/SPAN&gt;&amp;nbsp; in KDS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 21:07:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Import-project-from-Code-Warrior-to-Kinetis-Design-Studio/m-p/450617#M2389</guid>
      <dc:creator>vitaliysiplichu</dc:creator>
      <dc:date>2015-05-20T21:07:18Z</dc:date>
    </item>
  </channel>
</rss>