<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMPR121 disable baseline filtering ?!</title>
    <link>https://community.nxp.com/t5/Sensors/MPR121-disable-baseline-filtering/m-p/439978#M2230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in my scenario i want to use the MPR121 for LONG time touch/body detection. The Problem is that the baseline-filter decreases my baseline-value an after a few minutes and the body will not be detected anymore. My Thresholds are 10 for touch and 5 for release so when the filter decreases the value for 4 (is this configurable ? its always 4 even if i change NHDL and NHDT) the baseline - filtered value is not &amp;lt; threshold anymore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The solution to set the NCL and FDL both to 0xFF only create a delay but will not solve the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to deactivate the filter ?&amp;nbsp; Or set the value which decreases the baseline to zero ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2015 09:42:19 GMT</pubDate>
    <dc:creator>felixover</dc:creator>
    <dc:date>2015-05-18T09:42:19Z</dc:date>
    <item>
      <title>MPR121 disable baseline filtering ?!</title>
      <link>https://community.nxp.com/t5/Sensors/MPR121-disable-baseline-filtering/m-p/439978#M2230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in my scenario i want to use the MPR121 for LONG time touch/body detection. The Problem is that the baseline-filter decreases my baseline-value an after a few minutes and the body will not be detected anymore. My Thresholds are 10 for touch and 5 for release so when the filter decreases the value for 4 (is this configurable ? its always 4 even if i change NHDL and NHDT) the baseline - filtered value is not &amp;lt; threshold anymore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The solution to set the NCL and FDL both to 0xFF only create a delay but will not solve the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to deactivate the filter ?&amp;nbsp; Or set the value which decreases the baseline to zero ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 09:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR121-disable-baseline-filtering/m-p/439978#M2230</guid>
      <dc:creator>felixover</dc:creator>
      <dc:date>2015-05-18T09:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: MPR121 disable baseline filtering ?!</title>
      <link>https://community.nxp.com/t5/Sensors/MPR121-disable-baseline-filtering/m-p/439979#M2231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Felix Over,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can disable the baseline tracking by setting CL bit on Register 0x5E to [01] as can be seen on page 16 of the &lt;A href="http://cache.freescale.com/files/sensors/doc/data_sheet/MPR121.pdf"&gt;MPR121 Datasheet&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other thing you can do is to change the filters configuration. Check the Application Note &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN3891.pdf?fsrch=1&amp;amp;sr=2."&gt;AN3891&lt;/A&gt; for filters configuration information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 16:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPR121-disable-baseline-filtering/m-p/439979#M2231</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-05-27T16:44:23Z</dc:date>
    </item>
  </channel>
</rss>