<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic way to increase Sensitivity in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436874#M2168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Thanks to a kind reply, 9-axi sensor board is working well. Roll, pitch, Yaw values is relatively accurate.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but our sensor board is moving very slowly. and i dont need to run more than 100deg/s&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so if i can, i want to add more accuracy than fast response.&lt;/P&gt;&lt;P&gt;I edited acc, gyro sensor register to increase sensitivty ( acc : 2g -&amp;gt; g, gyro : 2000dps/LSB -&amp;gt; 250dps/LSB )&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there another way to increase sensitivity by using software or by using register ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:12:01 GMT</pubDate>
    <dc:creator>timronaldo</dc:creator>
    <dc:date>2026-02-03T21:12:01Z</dc:date>
    <item>
      <title>way to increase Sensitivity</title>
      <link>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436874#M2168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Thanks to a kind reply, 9-axi sensor board is working well. Roll, pitch, Yaw values is relatively accurate.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but our sensor board is moving very slowly. and i dont need to run more than 100deg/s&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so if i can, i want to add more accuracy than fast response.&lt;/P&gt;&lt;P&gt;I edited acc, gyro sensor register to increase sensitivty ( acc : 2g -&amp;gt; g, gyro : 2000dps/LSB -&amp;gt; 250dps/LSB )&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there another way to increase sensitivity by using software or by using register ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436874#M2168</guid>
      <dc:creator>timronaldo</dc:creator>
      <dc:date>2026-02-03T21:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: way to increase Sensitivity</title>
      <link>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436875#M2169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your questions covers both sensitivity (ability to detect a change in orientation) and accuracy (error in the orientation estimate). You should also be aware of sensor noise which makes it difficult to separate a real change from random noise.&lt;/P&gt;&lt;P&gt;The changes you've made will increase sensitivity.&lt;/P&gt;&lt;P&gt;The overall accuracy of the system is determined by the accuracy of the factory accelerometer calibration and the real-time dynamic magnetic calibration. Of these two, the magnetic calibration will be the largest source of error.&lt;/P&gt;&lt;P&gt;To answer your question, there are no easy changes to improve your performance further.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 15:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436875#M2169</guid>
      <dc:creator>markpedley</dc:creator>
      <dc:date>2015-10-28T15:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: way to increase Sensitivity</title>
      <link>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436876#M2170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hopefully you changed the register settings AND the iCountsPerDegPerSec and fDegPerSecperCount in the pThisGyro structure in the gyro initialization code in drivers.c.&amp;nbsp; That should be all that is required.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 15:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436876#M2170</guid>
      <dc:creator>michaelestanley</dc:creator>
      <dc:date>2015-10-28T15:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: way to increase Sensitivity</title>
      <link>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436877#M2171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 23:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/way-to-increase-Sensitivity/m-p/436877#M2171</guid>
      <dc:creator>timronaldo</dc:creator>
      <dc:date>2015-10-28T23:01:49Z</dc:date>
    </item>
  </channel>
</rss>