<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックUsing MMA8452Q For tilt alarm detection</title>
    <link>https://community.nxp.com/t5/Sensors/Using-MMA8452Q-For-tilt-alarm-detection/m-p/427387#M2011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ALL,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;My project is to detect an angle of about +/- 40 ° relative to an initial position .&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a newbie in accelerometer domain&lt;SPAN lang="en"&gt; and the concepts covered in the data sheet are not very clear in my mind&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I'll try to ask simple questions have simple answers&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;1°) Is it possible to do that with MMA8452Q ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;2°) &lt;SPAN lang="en"&gt;Is there an application note that clearly explains the implementation of my project with the MMA8452Q ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;thank you very much&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Sincerely&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jérôme.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:56:51 GMT</pubDate>
    <dc:creator>mat66mat</dc:creator>
    <dc:date>2026-02-03T22:56:51Z</dc:date>
    <item>
      <title>Using MMA8452Q For tilt alarm detection</title>
      <link>https://community.nxp.com/t5/Sensors/Using-MMA8452Q-For-tilt-alarm-detection/m-p/427387#M2011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ALL,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;My project is to detect an angle of about +/- 40 ° relative to an initial position .&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a newbie in accelerometer domain&lt;SPAN lang="en"&gt; and the concepts covered in the data sheet are not very clear in my mind&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I'll try to ask simple questions have simple answers&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;1°) Is it possible to do that with MMA8452Q ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;2°) &lt;SPAN lang="en"&gt;Is there an application note that clearly explains the implementation of my project with the MMA8452Q ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;thank you very much&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Sincerely&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jérôme.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Using-MMA8452Q-For-tilt-alarm-detection/m-p/427387#M2011</guid>
      <dc:creator>mat66mat</dc:creator>
      <dc:date>2026-02-03T22:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using MMA8452Q For tilt alarm detection</title>
      <link>https://community.nxp.com/t5/Sensors/Using-MMA8452Q-For-tilt-alarm-detection/m-p/427388#M2012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Yes, the MMA8452Q have an embedded orientation detection feature that can be used for a Tilt alarm detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Yes, there are some documents that can help you with this application:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;2.1) &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4068.pdf"&gt;AN4068&lt;/A&gt; “Embedded Orientation Detection Using the MMA8451, 2, 3Q”&lt;/LI&gt;&lt;LI&gt;2.2) &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN3461.pdf"&gt;AN3461&lt;/A&gt; “Tilt Sensing Using Three-Axis Accelerometer”&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, if a +/- 45° angle detection can work for your application, I would like to recommend you to use the &lt;A href="http://cache.freescale.com/files/sensors/doc/data_sheet/MMA8491Q.pdf"&gt;MMA8491Q&lt;/A&gt;, this accelerometer device as a 45° Tilt Sensor, it offers extreme ease of implementation by using a single line output per axis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 15:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Using-MMA8452Q-For-tilt-alarm-detection/m-p/427388#M2012</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-06-24T15:57:18Z</dc:date>
    </item>
  </channel>
</rss>