<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: MPXV5050GP - Pin functions and package</title>
    <link>https://community.nxp.com/t5/Sensors/MPXV5050GP-Pin-functions-and-package/m-p/418464#M1882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prathamesh Dhanpalwar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Package used in the MPXV5050GP is a SOP-8 with a case no. 1369-01, package dimensions of this device can be found &lt;A href="http://cache.freescale.com/files/shared/doc/package_info/98ASA99303D.pdf"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As stated in Document &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-97353"&gt;DOC-97353&lt;/A&gt;, the difference between style 1 and style 2 in the package dimensions is due to the two main families of pressure sensors Freescale offers.&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;Style 1 is usually applicable for all MPXx10, MPXx53 and MPXx2000-series SOP Type package pressure sensors featuring differential outputs.&lt;BR /&gt; &lt;BR /&gt; Style 2 is applicable for all MPXx4000-series, MPXx5000-series, MPXx6000-series, MPXx7000-series integrated devices in surface mount packages featuring single ended outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So for the case of the MPXV5050GP, case no. 1369-01, you should use Style 2:&lt;/P&gt;&lt;P&gt;Pin 1: N/C&lt;/P&gt;&lt;P&gt;Pin 2: Vs&lt;/P&gt;&lt;P&gt;Pin3: GND&lt;/P&gt;&lt;P&gt;Pin 4: Vout&lt;/P&gt;&lt;P&gt;Pin 5: N/C&lt;/P&gt;&lt;P&gt;Pin 6: N/C&lt;/P&gt;&lt;P&gt;Pin 7: N/C&lt;/P&gt;&lt;P&gt;Pin 8: N/C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, you can find a 3D Step design for this package &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95443"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2015 16:03:07 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2015-06-22T16:03:07Z</dc:date>
    <item>
      <title>MPXV5050GP - Pin functions and package</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5050GP-Pin-functions-and-package/m-p/418463#M1881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I am thinking of using MPXV5050GP and the datasheet says that it is of SOP-8 package. But the dimensions are quite different than the usual SOP-8 package. Also, the pin functions are based on style 1 and style 2, but the datasheet doesn't say which one applies to MPXV5050GP. Can anyone throw light on this please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;A href="https://community.nxp.com/space/11146" target="_blank"&gt;Sensors&lt;/A&gt;​&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5050GP-Pin-functions-and-package/m-p/418463#M1881</guid>
      <dc:creator>prathameshdhanp</dc:creator>
      <dc:date>2026-02-03T22:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV5050GP - Pin functions and package</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5050GP-Pin-functions-and-package/m-p/418464#M1882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prathamesh Dhanpalwar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Package used in the MPXV5050GP is a SOP-8 with a case no. 1369-01, package dimensions of this device can be found &lt;A href="http://cache.freescale.com/files/shared/doc/package_info/98ASA99303D.pdf"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As stated in Document &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-97353"&gt;DOC-97353&lt;/A&gt;, the difference between style 1 and style 2 in the package dimensions is due to the two main families of pressure sensors Freescale offers.&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;Style 1 is usually applicable for all MPXx10, MPXx53 and MPXx2000-series SOP Type package pressure sensors featuring differential outputs.&lt;BR /&gt; &lt;BR /&gt; Style 2 is applicable for all MPXx4000-series, MPXx5000-series, MPXx6000-series, MPXx7000-series integrated devices in surface mount packages featuring single ended outputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So for the case of the MPXV5050GP, case no. 1369-01, you should use Style 2:&lt;/P&gt;&lt;P&gt;Pin 1: N/C&lt;/P&gt;&lt;P&gt;Pin 2: Vs&lt;/P&gt;&lt;P&gt;Pin3: GND&lt;/P&gt;&lt;P&gt;Pin 4: Vout&lt;/P&gt;&lt;P&gt;Pin 5: N/C&lt;/P&gt;&lt;P&gt;Pin 6: N/C&lt;/P&gt;&lt;P&gt;Pin 7: N/C&lt;/P&gt;&lt;P&gt;Pin 8: N/C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, you can find a 3D Step design for this package &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95443"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 16:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5050GP-Pin-functions-and-package/m-p/418464#M1882</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-06-22T16:03:07Z</dc:date>
    </item>
  </channel>
</rss>