<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックLifetime calculation MPXV5010</title>
    <link>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413133#M1789</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are planning to use a MPXV5010 in an industrial application, where it would serve as a programmable pressure switch in an "air-barrier", replacing the currently used pneumatic pressure amplifiers. However, in order to verify that the sensor is suitable for this application we need a good estimation for the expected lifetime, as the system is required to work without failure for several years (in this application a failure of the sensor would mean a total failure or loss of sensitivity / drift &amp;gt; 20 %, smaller changes in sensitivity / drift could be compensated for). Typical operation conditions would be:&lt;/P&gt;&lt;P&gt;1.) Operation with dried and filtered air.&lt;/P&gt;&lt;P&gt;2.) Ambient / air temperature 10...50 degrees Celsius.&lt;/P&gt;&lt;P&gt;3.) Input pressure varying between 0...5 kPa, i.e. up to 50 % of nominal input pressure range.&lt;/P&gt;&lt;P&gt;4.) Frequency of pressure change approximately 0.5...0.05 Hz.&lt;/P&gt;&lt;P&gt;5.) Input pressure rise and drop within a few ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;a) Is there a formula to calculate the estimated lifetime as a function of ambient / air temperature, input pressure change, frequency of pressure change and possibly slew rate of pressure change? We could not find any information about the lifetime in the documentation available.&lt;/P&gt;&lt;P&gt;b) Would it make a difference for the lifetime under the above conditions when a MPVZ5010 would be used instead? We are aware that it would reduce the risk of premature failure due to high humidity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:48:20 GMT</pubDate>
    <dc:creator>christianwieber</dc:creator>
    <dc:date>2026-02-03T22:48:20Z</dc:date>
    <item>
      <title>Lifetime calculation MPXV5010</title>
      <link>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413133#M1789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are planning to use a MPXV5010 in an industrial application, where it would serve as a programmable pressure switch in an "air-barrier", replacing the currently used pneumatic pressure amplifiers. However, in order to verify that the sensor is suitable for this application we need a good estimation for the expected lifetime, as the system is required to work without failure for several years (in this application a failure of the sensor would mean a total failure or loss of sensitivity / drift &amp;gt; 20 %, smaller changes in sensitivity / drift could be compensated for). Typical operation conditions would be:&lt;/P&gt;&lt;P&gt;1.) Operation with dried and filtered air.&lt;/P&gt;&lt;P&gt;2.) Ambient / air temperature 10...50 degrees Celsius.&lt;/P&gt;&lt;P&gt;3.) Input pressure varying between 0...5 kPa, i.e. up to 50 % of nominal input pressure range.&lt;/P&gt;&lt;P&gt;4.) Frequency of pressure change approximately 0.5...0.05 Hz.&lt;/P&gt;&lt;P&gt;5.) Input pressure rise and drop within a few ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;a) Is there a formula to calculate the estimated lifetime as a function of ambient / air temperature, input pressure change, frequency of pressure change and possibly slew rate of pressure change? We could not find any information about the lifetime in the documentation available.&lt;/P&gt;&lt;P&gt;b) Would it make a difference for the lifetime under the above conditions when a MPVZ5010 would be used instead? We are aware that it would reduce the risk of premature failure due to high humidity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413133#M1789</guid>
      <dc:creator>christianwieber</dc:creator>
      <dc:date>2026-02-03T22:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: Lifetime calculation MPXV5010</title>
      <link>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413134#M1790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may create Service Request via Freescale Web in order to get the information requested. &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/training/sales-and-support:SUPPORTHOME" title="https://www.freescale.com/webapp/training/sales-and-support:SUPPORTHOME"&gt;Sales and Support|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day. :smileyhappy:&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 16:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413134#M1790</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-09-02T16:58:02Z</dc:date>
    </item>
    <item>
      <title>Re: Lifetime calculation MPXV5010</title>
      <link>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413135#M1791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your feedback, I already created a service request as recommended by you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christian Wieber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 01:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Lifetime-calculation-MPXV5010/m-p/413135#M1791</guid>
      <dc:creator>christianwieber</dc:creator>
      <dc:date>2015-09-03T01:58:02Z</dc:date>
    </item>
  </channel>
</rss>