<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックMPXV5004 Sensor Application question</title>
    <link>https://community.nxp.com/t5/Sensors/MPXV5004-Sensor-Application-question/m-p/405687#M1658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I'm from a Commercial Glass &amp;amp; Dishwasher manufacture &amp;amp; we are looking at replacing our old diaphragm based pressure switches to the MPXV5004 pressure sensor with our control board, with reading the Datasheet it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Internal reliability and qualification test for dry air, and other media, are available from the factory. Contact the factory for information regarding media tolerance in your application". &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so my question is we can provide clean air to the sensor through an Air-Bell, but it wont be dry it will have around 60-70% humidity as we use hot water in the machines. will this affect the sensors reliability or longevity?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, are there other sensors that could be used? or a recommended way that we could connect the tube from the Air-Bell to the pressure sensor?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Damien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 22:29:12 GMT</pubDate>
    <dc:creator>damienberry</dc:creator>
    <dc:date>2026-02-03T22:29:12Z</dc:date>
    <item>
      <title>MPXV5004 Sensor Application question</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5004-Sensor-Application-question/m-p/405687#M1658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I'm from a Commercial Glass &amp;amp; Dishwasher manufacture &amp;amp; we are looking at replacing our old diaphragm based pressure switches to the MPXV5004 pressure sensor with our control board, with reading the Datasheet it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Internal reliability and qualification test for dry air, and other media, are available from the factory. Contact the factory for information regarding media tolerance in your application". &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so my question is we can provide clean air to the sensor through an Air-Bell, but it wont be dry it will have around 60-70% humidity as we use hot water in the machines. will this affect the sensors reliability or longevity?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, are there other sensors that could be used? or a recommended way that we could connect the tube from the Air-Bell to the pressure sensor?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Damien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5004-Sensor-Application-question/m-p/405687#M1658</guid>
      <dc:creator>damienberry</dc:creator>
      <dc:date>2026-02-03T22:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV5004 Sensor Application question</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5004-Sensor-Application-question/m-p/405688#M1659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for using our community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could protect the sensor using a high viscosity silicone. Please, take a look at the following thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A _jive_internal="true" data-containerid="11146" data-containertype="14" data-content-finding="Community" data-objectid="509994" data-objecttype="2" href="https://community.nxp.com/message/509994#509994"&gt;Re: 30% of MPXM2202GS failed within 2 months after installation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2015 16:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5004-Sensor-Application-question/m-p/405688#M1659</guid>
      <dc:creator>Joshevelle</dc:creator>
      <dc:date>2015-06-17T16:10:52Z</dc:date>
    </item>
  </channel>
</rss>