<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Hi, does Freescale have a multitouch resistive xy sensor?</title>
    <link>https://community.nxp.com/t5/Sensors/Hi-does-Freescale-have-a-multitouch-resistive-xy-sensor/m-p/398744#M1564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And if so can it be made into custom shapes/sizes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also - would be advantageous to be force-pressure sensitive?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a product like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2015 05:10:03 GMT</pubDate>
    <dc:creator>rupertbg</dc:creator>
    <dc:date>2015-05-27T05:10:03Z</dc:date>
    <item>
      <title>Hi, does Freescale have a multitouch resistive xy sensor?</title>
      <link>https://community.nxp.com/t5/Sensors/Hi-does-Freescale-have-a-multitouch-resistive-xy-sensor/m-p/398744#M1564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And if so can it be made into custom shapes/sizes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also - would be advantageous to be force-pressure sensitive?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a product like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 05:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Hi-does-Freescale-have-a-multitouch-resistive-xy-sensor/m-p/398744#M1564</guid>
      <dc:creator>rupertbg</dc:creator>
      <dc:date>2015-05-27T05:10:03Z</dc:date>
    </item>
    <item>
      <title>Re: Hi, does Freescale have a multitouch resistive xy sensor?</title>
      <link>https://community.nxp.com/t5/Sensors/Hi-does-Freescale-have-a-multitouch-resistive-xy-sensor/m-p/398745#M1565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rupert Bryant-Greene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the Freescale &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CRTOUCH&amp;amp;fsrch=1&amp;amp;sr=6&amp;amp;pageNum=1"&gt;CRTOUCH&lt;/A&gt; Touch Sensing Platform is a Ready play solution that integrates standard X, Y resistive touch screen detection, pressure detection on 4 and 5 wires, single and double touch detection, gesture detection and 4 capacitive electrodes independent from touch screen.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 15:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Hi-does-Freescale-have-a-multitouch-resistive-xy-sensor/m-p/398745#M1565</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-05-27T15:39:18Z</dc:date>
    </item>
  </channel>
</rss>