<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: Re: S12DP512 interface with 3.3V devices.</title>
    <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398165#M1559</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pulling the bus to 5V is not really a solution since both the SDA and SCL pins are not tolerant of voltages higher than VDDIO + 0.3V (3.6V max).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;However, looking at the MC9S12DP512 specs, the minimum voltage for a high level is 0.65*Vdd, which is 3.25V at a 5V supply. So, if you pull the I2C bus to 3.3V, you might not need an I2C level shifter.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 May 2015 10:39:34 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2015-05-05T10:39:34Z</dc:date>
    <item>
      <title>S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398162#M1556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use S12DP512 to interface with a pressure sensor and accelerometer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The voltage of these sensors Vdd are 3.3V and the Vdd of S12DP512 is 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can the MCU interface with these sensors? Should I need a level shifter? or They are TTL compatible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your helping.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 10:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398162#M1556</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2015-05-04T10:15:46Z</dc:date>
    </item>
    <item>
      <title>Re: S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398163#M1557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;You did not specify which sensors you are going to use, but in general I would suggest using both a logic level converter and a 3.3V regulator to allow everything to run at the proper voltages.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM style="font-size: 13px; font-family: Arial, sans-serif; color: #333333;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;&lt;EM style="font-weight: inherit; font-family: inherit;"&gt;PS:&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space"&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;I&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;f my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 11:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398163#M1557</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-05-04T11:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398164#M1558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to connect to 3 I2C sensors. 1 of them is 5.5Vdc max. so &lt;/P&gt;&lt;P&gt;there is no problem of it. The others are 3.6Vdc max.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are :&lt;/P&gt;&lt;P&gt;1. Freescale FXLS8471Q (Linear Accelerometer)&lt;/P&gt;&lt;P&gt;2. Measurement Specialties MS5607-02BA03 (Barometric Pressure Sensor)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot confirm are they TTL compatible. If yes, I think I don't need a &lt;/P&gt;&lt;P&gt;level shifter IC. Do you have any recommendation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Really thanks for your helping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 01:03:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398164#M1558</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2015-05-05T01:03:00Z</dc:date>
    </item>
    <item>
      <title>Re: Re: S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398165#M1559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pulling the bus to 5V is not really a solution since both the SDA and SCL pins are not tolerant of voltages higher than VDDIO + 0.3V (3.6V max).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;However, looking at the MC9S12DP512 specs, the minimum voltage for a high level is 0.65*Vdd, which is 3.25V at a 5V supply. So, if you pull the I2C bus to 3.3V, you might not need an I2C level shifter.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 10:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398165#M1559</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-05-05T10:39:34Z</dc:date>
    </item>
    <item>
      <title>Re: S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398166#M1560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can understand your theory. That mean MCU side can accept the high &lt;/P&gt;&lt;P&gt;signal from sensor once the voltage level is higher than 3.25V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, can the sensor accept the high signal from the MCU? The VDD of &lt;/P&gt;&lt;P&gt;the sensor is 3.6V max. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Henry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 10:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398166#M1560</guid>
      <dc:creator>monstor</dc:creator>
      <dc:date>2015-05-05T10:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: S12DP512 interface with 3.3V devices.</title>
      <link>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398167#M1561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Henry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;I do not quite understand what you mean by „&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d; background: white;"&gt;can the sensor accept the high signal from the MCU&lt;/SPAN&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;“. &lt;/SPAN&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;The trick is to connect the pull-up resistors to the lower of the two voltages, in our case to 3.3V. When the output transistor is off, the resistor connects the pin to 3.3V (not to 5V).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="CS" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 11:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/S12DP512-interface-with-3-3V-devices/m-p/398167#M1561</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-05-05T11:45:14Z</dc:date>
    </item>
  </channel>
</rss>