<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What is the proper method for retrieving samples from the CRTouch using the FIFO? in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/What-is-the-proper-method-for-retrieving-samples-from-the/m-p/392224#M1451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reading the CRTouch Datasheet, I am not sure how the FIFO buffer gets read using interrupts.&amp;nbsp; I understand that the FIFO watermark can trigger an interrupt to the CPU. But, once the FIFO interrupt has occurred and you send the command to read the FIFO buffer; what is the method for reading the FIFO so that the CPU doesn't run ahead of the 100Kbs rate of the CRTouch?&amp;nbsp; I would like to use an interrupt method, but it looks like I have to use a polling method, is that correct? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The docs don't give a description of reading the FIFO.&amp;nbsp; Maybe I'm missing something basic... my apologies in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Duane&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:06:04 GMT</pubDate>
    <dc:creator>wildhorsemusic</dc:creator>
    <dc:date>2026-02-03T23:06:04Z</dc:date>
    <item>
      <title>What is the proper method for retrieving samples from the CRTouch using the FIFO?</title>
      <link>https://community.nxp.com/t5/Sensors/What-is-the-proper-method-for-retrieving-samples-from-the/m-p/392224#M1451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reading the CRTouch Datasheet, I am not sure how the FIFO buffer gets read using interrupts.&amp;nbsp; I understand that the FIFO watermark can trigger an interrupt to the CPU. But, once the FIFO interrupt has occurred and you send the command to read the FIFO buffer; what is the method for reading the FIFO so that the CPU doesn't run ahead of the 100Kbs rate of the CRTouch?&amp;nbsp; I would like to use an interrupt method, but it looks like I have to use a polling method, is that correct? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The docs don't give a description of reading the FIFO.&amp;nbsp; Maybe I'm missing something basic... my apologies in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Duane&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/What-is-the-proper-method-for-retrieving-samples-from-the/m-p/392224#M1451</guid>
      <dc:creator>wildhorsemusic</dc:creator>
      <dc:date>2026-02-03T23:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: What is the proper method for retrieving samples from the CRTouch using the FIFO?</title>
      <link>https://community.nxp.com/t5/Sensors/What-is-the-proper-method-for-retrieving-samples-from-the/m-p/392225#M1452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Duane Owens,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, unfortunately it is not possible to read the FIFO buffer using Interrupt method, you would need to use a polling method to read it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 21:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/What-is-the-proper-method-for-retrieving-samples-from-the/m-p/392225#M1452</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-11-10T21:48:57Z</dc:date>
    </item>
  </channel>
</rss>