<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPL3115A2 Turn-on time specification in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Turn-on-time-specification/m-p/382959#M1346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the Electrical Characteristics section of the mpl3115a2 data sheet (page 6),&lt;/P&gt;&lt;P&gt;item 14 is the Turn-on time.&amp;nbsp; In 128os mode, it's specified at 1000 ms.&lt;/P&gt;&lt;P&gt;This is the amount of time you have to wait for "valid data" after exiting&lt;/P&gt;&lt;P&gt;standby mode and entering active mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see this delay implemented in any of the sample mpl3115a2 drivers posted on&lt;/P&gt;&lt;P&gt;the internet or on this website.&amp;nbsp;&amp;nbsp; I would expect to see code as follows, with a 1000ms&lt;/P&gt;&lt;P&gt;delay after leaving standby and entering active mode:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I2C_WriteRegister(MPL3115A2_I2C_ADDRESS, CTRL_REG1, 0xB9);&amp;nbsp;&amp;nbsp; // Active altitude mode, OSR = 128&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;delay_ms(1000);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;// then toggle the one-shot, wait for Data Ready, and read the data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the Turn-on Time specification real, or can it safely be ignored ?&lt;/P&gt;&lt;P&gt;-------------------&lt;/P&gt;&lt;P&gt;Also can the forum Moderator please contact me.&amp;nbsp; I set my profile&lt;/P&gt;&lt;P&gt;to use my "handle" instead of my name, but this setting is ignored.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:07:06 GMT</pubDate>
    <dc:creator>jeff_1234</dc:creator>
    <dc:date>2026-02-03T23:07:06Z</dc:date>
    <item>
      <title>MPL3115A2 Turn-on time specification</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Turn-on-time-specification/m-p/382959#M1346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the Electrical Characteristics section of the mpl3115a2 data sheet (page 6),&lt;/P&gt;&lt;P&gt;item 14 is the Turn-on time.&amp;nbsp; In 128os mode, it's specified at 1000 ms.&lt;/P&gt;&lt;P&gt;This is the amount of time you have to wait for "valid data" after exiting&lt;/P&gt;&lt;P&gt;standby mode and entering active mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see this delay implemented in any of the sample mpl3115a2 drivers posted on&lt;/P&gt;&lt;P&gt;the internet or on this website.&amp;nbsp;&amp;nbsp; I would expect to see code as follows, with a 1000ms&lt;/P&gt;&lt;P&gt;delay after leaving standby and entering active mode:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I2C_WriteRegister(MPL3115A2_I2C_ADDRESS, CTRL_REG1, 0xB9);&amp;nbsp;&amp;nbsp; // Active altitude mode, OSR = 128&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;delay_ms(1000);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;// then toggle the one-shot, wait for Data Ready, and read the data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the Turn-on Time specification real, or can it safely be ignored ?&lt;/P&gt;&lt;P&gt;-------------------&lt;/P&gt;&lt;P&gt;Also can the forum Moderator please contact me.&amp;nbsp; I set my profile&lt;/P&gt;&lt;P&gt;to use my "handle" instead of my name, but this setting is ignored.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-Turn-on-time-specification/m-p/382959#M1346</guid>
      <dc:creator>jeff_1234</dc:creator>
      <dc:date>2026-02-03T23:07:06Z</dc:date>
    </item>
  </channel>
</rss>