<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックFXOS8700 accel transient threshold resolution in per-axis mode</title>
    <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354853#M1045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the FXOS8700 with the accelerometer transient detection feature. The data sheet shows two ways to set the threshold:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use TRANSIENT_THS which has a resolution of 63 mg/LSB and the same threshold would be used for all axes&lt;/LI&gt;&lt;LI&gt;Use A_FFMT_THS_* by setting high bit of A_FFMT_THS_Y_MSB and then you can set per-axis thresholds&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the resolution of the A_FFMT_THS_* registers when they are used to set the threshold? From my tests, it looks like it is also 63 mg. The lowest two bits of each register aren't used so the values have to be shifted left by two bits, but otherwise it appears that the resolution is also 63 mg? I can't find specific mention in the datasheet and I have to admit I was hoping for a higher-resolution threshold so that it could be set lower than 63 mg.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:07:34 GMT</pubDate>
    <dc:creator>nickv</dc:creator>
    <dc:date>2026-02-03T21:07:34Z</dc:date>
    <item>
      <title>FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354853#M1045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the FXOS8700 with the accelerometer transient detection feature. The data sheet shows two ways to set the threshold:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use TRANSIENT_THS which has a resolution of 63 mg/LSB and the same threshold would be used for all axes&lt;/LI&gt;&lt;LI&gt;Use A_FFMT_THS_* by setting high bit of A_FFMT_THS_Y_MSB and then you can set per-axis thresholds&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the resolution of the A_FFMT_THS_* registers when they are used to set the threshold? From my tests, it looks like it is also 63 mg. The lowest two bits of each register aren't used so the values have to be shifted left by two bits, but otherwise it appears that the resolution is also 63 mg? I can't find specific mention in the datasheet and I have to admit I was hoping for a higher-resolution threshold so that it could be set lower than 63 mg.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354853#M1045</guid>
      <dc:creator>nickv</dc:creator>
      <dc:date>2026-02-03T21:07:34Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354854#M1046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the resolution will not improve using the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px; font-style: normal; font-weight: normal; text-align: left; text-indent: 0px;"&gt;A_FFMT_THS_* settings. Resolution is fixed at 63 mg/LSB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 21:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354854#M1046</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-03-26T21:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354855#M1047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;The A_FFMT_THS_X/Y/Z MSB and LSB registers (0x73 – 0x78) are used by both the freefall/motion detection and the transient detection functional blocks to set independent threshold values for each axis with the same resolution as the accelerometer &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;output data determined by fs[1:0] bits of the XYZ_DATA_CFG register. For example, if fs[1:0] = 0b00 (±2g), the resolution of the A_FFMT_THS_X/Y/Z registers is 0.244 mg/LSB, if fs[1:0] = 0b10 (±8g), the resolution is 0.976 mg/LSB. As you correctly noted, the threshold values stored in the A_FFMT_THS_X/Y/Z registers are used by the t&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif;"&gt;ransient detection &lt;/SPAN&gt;functional block if the a_ffmt_trans_ths_en bit of the A_FFMT_THS_Y_MSB register is set high. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;Example setting for Z &amp;gt; 31.25mg, 2g mode, 800Hz ODR, High resolution and Low noise:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG2, 0x40);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="color: #3f7f5f; font-family: Consolas; font-size: 13.3333330154419px;"&gt;// R&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;eset all registers to POR values&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;Pause(0x631);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// ~1ms delay&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, XYZ_DATA_CFG_REG, 0x00);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// ±2g range with 0.244mg/LSB&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, M_CTRL_REG1, 0x00);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Accelerometer only mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, TRANSIENT_CFG_REG, 0x18);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Enable transient detection for Z axis, latch enabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, A_FFMT_THSY_MSB_REG, 0x80);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Use threshold values from A_FFMT_THS_Z registers &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, A_FFMT_THSZ_MSB_REG, 0x02);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Set threshold to about 31.25mg (31.25mg / 0.244mg = 128 = 0b10000000)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, A_FFMT_THSZ_LSB_REG, 0x00);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, TRANSIENT_COUNT_REG , 0x00);&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Set debounce to zero &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG2, 0x02);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// High Resolution mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG3, 0x00);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Push-pull, active low interrupt &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG4, 0x20);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// Transient interrupt enabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG5, 0x20);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;/&lt;SPAN style="color: #3f7f5f; font-family: Consolas; font-size: 13.3333330154419px;"&gt;/&lt;/SPAN&gt; Transient interrupt routed to INT1 - PTD4 &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG1, 0x05);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;// ODR = 800Hz, Reduced noise, Active mode &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif; font-size: 13.3333330154419px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif; font-size: 13.3333330154419px;"&gt;I will send you the complete example project on Monday as soon as I double check it in the lab.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif; font-size: 13.3333330154419px;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif; font-size: 13.3333330154419px;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: Helvetica, sans-serif; font-size: 13.3333330154419px;"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 10:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354855#M1047</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-03-27T10:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354856#M1048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any update on your test?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2015 17:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354856#M1048</guid>
      <dc:creator>nickv</dc:creator>
      <dc:date>2015-04-01T17:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354857#M1049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;I have done some more investigation into this and tried different settings. &lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;It seems like the resolution of the A_FFMT_THS registers when used for transient detection (a_ffmt_trans_ths_en = 1) is indeed fixed to 62.5 mg and is not determined by the fs[1:0] bits of the XYZ_DATA_CFG register.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;I have requested assistance from the design team to verify the implementation on the ASIC. I should have a final answer by tomorrow.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Helvetica','sans-serif'; color: #3d3d3d;"&gt;Tomas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2015 12:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354857#M1049</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-04-02T12:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: Re: FXOS8700 accel transient threshold resolution in per-axis mode</title>
      <link>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354858#M1050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reviewing it with the design team, I confirm that the transient threshold resolution is fixed to 62.5 mg. For a_ffmt_trans_ths_en = 1, the ASIC uses reg 0x1F[6:0] as the x-axis transient threshold, 0x75[0] and 0x76[7:2] as the y-axis threshold and 0x77[0] and 0x78[7:2] as the z-axis threshold.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet is being updated and should be available on the web within the next few days. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry it has taken so long to clarify it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 08:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXOS8700-accel-transient-threshold-resolution-in-per-axis-mode/m-p/354858#M1050</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2015-04-08T08:54:53Z</dc:date>
    </item>
  </channel>
</rss>