<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックIs it possible to add extra applets to the SE050</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946042#M99</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I'm reaching you to clarify some of the capabilities that I understand the SE050 might have.&lt;/P&gt;&lt;P&gt;According to the "AN12413&amp;nbsp;API description SE050 IoT Applet", SE050 is being executed on top of JCOP 4.7.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to use the 50K memory in the device to extend the functionaly of the chip by adding extra applets?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Sep 2019 10:20:42 GMT</pubDate>
    <dc:creator>umujika</dc:creator>
    <dc:date>2019-09-04T10:20:42Z</dc:date>
    <item>
      <title>Is it possible to add extra applets to the SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946042#M99</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I'm reaching you to clarify some of the capabilities that I understand the SE050 might have.&lt;/P&gt;&lt;P&gt;According to the "AN12413&amp;nbsp;API description SE050 IoT Applet", SE050 is being executed on top of JCOP 4.7.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to use the 50K memory in the device to extend the functionaly of the chip by adding extra applets?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 10:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946042#M99</guid>
      <dc:creator>umujika</dc:creator>
      <dc:date>2019-09-04T10:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add extra applets to the SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946043#M100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;Technically it is possible but it depends on an agreement between NXP and the customer &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;–&lt;SPAN&gt; finally the volume makes the difference.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;&lt;SPAN&gt;Hope that makes sense,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;&lt;SPAN&gt;Have a great day,&lt;BR /&gt;Kan &lt;BR /&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 05:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946043#M100</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-11T05:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add extra applets to the SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946044#M101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kan,&lt;/P&gt;&lt;P&gt;Thanks for your answer, but I fear that your explanation leaves things still in the dark.&lt;/P&gt;&lt;P&gt;In a JCOP card, or in principle any JavaCard, as long as you have the necessary keys and rights it's possible to download additional applets and afterwards use them.&lt;/P&gt;&lt;P&gt;Is there a possibility, in the default unmodified SE050 that you could get from any official distributor, to download additional applets?&lt;/P&gt;&lt;P&gt;I'm not talking about adding NXP propietary applets (such as a MIFARE applet), but possibly other functionality, programmed by us.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 06:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946044#M101</guid>
      <dc:creator>umujika</dc:creator>
      <dc:date>2019-09-11T06:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add extra applets to the SE050</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946045#M102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the clarification! I understand now, but sorry that the 50 KB flash can only be used for secure data or key storage, so the answer is No.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 08:45:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Is-it-possible-to-add-extra-applets-to-the-SE050/m-p/946045#M102</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-12T08:45:21Z</dc:date>
    </item>
  </channel>
</rss>