<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: SE050 Minimal External Components</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941106#M89</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2019 19:44:12 GMT</pubDate>
    <dc:creator>wami</dc:creator>
    <dc:date>2019-10-31T19:44:12Z</dc:date>
    <item>
      <title>SE050 Minimal External Components</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941102#M85</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use an SE050 in an environemnt with very very limited space.&lt;/P&gt;&lt;P&gt;I do not want to use ISO14443 and ISO7816 and also not the Low-Power Feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just I2C and that's it for an µC:&lt;/P&gt;&lt;P&gt;I2C Pullup is at 2.4kOHM and I have put in the following components.&lt;/P&gt;&lt;P&gt;Is the connectivity right, and can I put the ISO14443 Atenna and ISO7816 Ports to GND/VCC without any pullup?&lt;/P&gt;&lt;P&gt;Anything else to take care about?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;&lt;P&gt;Michael&lt;span class="lia-inline-image-display-wrapper" image-alt="se050.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92836i6DBA2F9CA723FBF6/image-size/large?v=v2&amp;amp;px=999" role="button" title="se050.jpg" alt="se050.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 01:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941102#M85</guid>
      <dc:creator>wami</dc:creator>
      <dc:date>2019-10-03T01:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Minimal External Components</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941103#M86</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look to the following document for hardware overview, specially to chapter 6 for the schematics so that you can see the connections of the board:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12395-OM-SE050ARD_hardware_overview.pdf" title="https://www.nxp.com/docs/en/application-note/AN12395-OM-SE050ARD_hardware_overview.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12395-OM-SE050ARD_hardware_overview.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 17:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941103#M86</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-10-08T17:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Minimal External Components</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941104#M87</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;not to 100%. My question is more related on which parts can be removed.&lt;/P&gt;&lt;P&gt;In another Topic here there was a discussion in this Forum what to do with unused ports (GND or VCC) when not used. As I only use I²C and nothing else I have put them to VCC and GND as showed there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But my questions are:&lt;/P&gt;&lt;P&gt;- Do I have to use external PullUps or can I just directly connect them to VCC and GND (Internal Pull Ups in the Chip?)&lt;/P&gt;&lt;P&gt;- Can I remove the Coils (L1 to L4) if I do not use NFC? I assume it is for NFC usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to know if this is possible as the customer-design is already finished and now there is a need for security (as ususual ;-)) and we need to add the SE050 but with very very limited space available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not found any documentation about the Smart-Card Processor/Microcontroller used for the SE050-IoT Applet so I have no clue what is underneath and how the ports are designed/configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope you can help an clarify this a bit more.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 16:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941104#M87</guid>
      <dc:creator>wami</dc:creator>
      <dc:date>2019-10-11T16:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Minimal External Components</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941105#M88</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your minimum schematic is OK, I assume the I2C bus pull-ups are already somewhere else on the board?&lt;/P&gt;&lt;P&gt;The coils indeed can be removed when contact-less is not used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About pins being NC or needing some external connection we put some more data in another SE050 version datasheet (this data is not in the public version yet, contact-less interface not shown in this version, best to be connected to GND as done in your schematic). The table below is a little bit more verbose about the pins if they can be left open or not:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91381i261DBD91B4EE8896/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2019 21:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941105#M88</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-10-14T21:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Minimal External Components</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941106#M89</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 19:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Minimal-External-Components/m-p/941106#M89</guid>
      <dc:creator>wami</dc:creator>
      <dc:date>2019-10-31T19:44:12Z</dc:date>
    </item>
  </channel>
</rss>