<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックRe: AccessManager I2C device name configuration using argument</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/AccessManager-I2C-device-name-configuration-using-argument/m-p/1503180#M876</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202274"&gt;@ajitsj3&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actually so far there is no solution other than modifying the default I2C device name in AccessManager source code, but for your case , I would recommend modifying the default I2C device name in the source code to some symbol link file in the Linux file system, for example, "/dev/i2c-s" , and link i2c-s to different device name such as "/dev/i2c-2" or something like this. so you just need to change the default I2C device name just once.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope that makes sense,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 09 Aug 2022 09:28:24 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2022-08-09T09:28:24Z</dc:date>
    <item>
      <title>AccessManager I2C device name configuration using argument</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/AccessManager-I2C-device-name-configuration-using-argument/m-p/1502613#M875</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could we configure the I2C device name as "i2c-0" without making changes in the accessManager code?&lt;/P&gt;&lt;P&gt;We might have to use "i2c-1" as I2C device name for another device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So please let me know if there is a way to send this I2C device name as argument for accessManager?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Ajit S J&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 13:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/AccessManager-I2C-device-name-configuration-using-argument/m-p/1502613#M875</guid>
      <dc:creator>ajitsj3</dc:creator>
      <dc:date>2022-08-08T13:38:46Z</dc:date>
    </item>
    <item>
      <title>Re: AccessManager I2C device name configuration using argument</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/AccessManager-I2C-device-name-configuration-using-argument/m-p/1503180#M876</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202274"&gt;@ajitsj3&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actually so far there is no solution other than modifying the default I2C device name in AccessManager source code, but for your case , I would recommend modifying the default I2C device name in the source code to some symbol link file in the Linux file system, for example, "/dev/i2c-s" , and link i2c-s to different device name such as "/dev/i2c-2" or something like this. so you just need to change the default I2C device name just once.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope that makes sense,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 09:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/AccessManager-I2C-device-name-configuration-using-argument/m-p/1503180#M876</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-08-09T09:28:24Z</dc:date>
    </item>
  </channel>
</rss>