<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CLRC663ARD board and CLRC663PcSerial.3.6 test program in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1448416#M777</link>
    <description>&lt;P&gt;Hi!&lt;BR /&gt;I thought no one would answer!&lt;BR /&gt;The&amp;nbsp;&lt;SPAN&gt;serial baud&amp;nbsp;for RC663 is 115200!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Apr 2022 09:16:17 GMT</pubDate>
    <dc:creator>AlexBush</dc:creator>
    <dc:date>2022-04-25T09:16:17Z</dc:date>
    <item>
      <title>CLRC663ARD board and CLRC663PcSerial.3.6 test program</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1439927#M756</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I am currently developing a wireless rfid identification node via CLRC663ARD.&lt;/P&gt;&lt;P&gt;The interface of CLRC663ARD configured to uart connection.&lt;BR /&gt;CLRC663ARD connected to PC via usb-uart converter.&lt;/P&gt;&lt;P&gt;I tested the operation of the CLEV663ARD using the CLRC663PcSerial.3.6 test program.&lt;/P&gt;&lt;P&gt;And CLRC663PcSerial.3.6 freezes when executing any jcf script from the program.&lt;/P&gt;&lt;P&gt;The freeze looks like this: commands from the script are successfully executed one by one. And one command does not receive a response from the board, after which the command is repeated again. And so on indefinitely.&lt;/P&gt;&lt;P&gt;I have tested all the scripts from the CLRC663PcSerial.3.6.&lt;/P&gt;&lt;P&gt;Is this normal?&lt;/P&gt;</description>
      <pubDate>Wed, 06 Apr 2022 20:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1439927#M756</guid>
      <dc:creator>AlexBush</dc:creator>
      <dc:date>2022-04-06T20:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663ARD board and CLRC663PcSerial.3.6 test program</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1444723#M770</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is not normal.&lt;/P&gt;
&lt;P&gt;I would suggest you check the serial connection or the baud rate, default baud for RC663 is 115200.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sat, 16 Apr 2022 09:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1444723#M770</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-04-16T09:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663ARD board and CLRC663PcSerial.3.6 test program</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1448416#M777</link>
      <description>&lt;P&gt;Hi!&lt;BR /&gt;I thought no one would answer!&lt;BR /&gt;The&amp;nbsp;&lt;SPAN&gt;serial baud&amp;nbsp;for RC663 is 115200!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 09:16:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/CLRC663ARD-board-and-CLRC663PcSerial-3-6-test-program/m-p/1448416#M777</guid>
      <dc:creator>AlexBush</dc:creator>
      <dc:date>2022-04-25T09:16:17Z</dc:date>
    </item>
  </channel>
</rss>