<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic about the latest SE05x_MW file in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/about-the-latest-SE05x-MW-file/m-p/1448185#M775</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;in AN13030 v1.8 version, it metioned the latest&amp;nbsp;se05x recipe (se05x_4.0.0.bb) in the&amp;nbsp;the source code package (SE050-PLUG-TRUST-MW-v04.00.00.zip). but after checked with the package (se05x-PLUG-TRUST_mw_v04.01.01.zip),&amp;nbsp; the yocto bb is se05x_3.1.0.bb.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Could anyone provide the latest package to support&amp;nbsp;the latest&amp;nbsp;se05x recipe (se05x_4.0.0.bb) ? thanks!&lt;/P&gt;</description>
    <pubDate>Sun, 24 Apr 2022 10:06:12 GMT</pubDate>
    <dc:creator>tiger_gao</dc:creator>
    <dc:date>2022-04-24T10:06:12Z</dc:date>
    <item>
      <title>about the latest SE05x_MW file</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/about-the-latest-SE05x-MW-file/m-p/1448185#M775</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;in AN13030 v1.8 version, it metioned the latest&amp;nbsp;se05x recipe (se05x_4.0.0.bb) in the&amp;nbsp;the source code package (SE050-PLUG-TRUST-MW-v04.00.00.zip). but after checked with the package (se05x-PLUG-TRUST_mw_v04.01.01.zip),&amp;nbsp; the yocto bb is se05x_3.1.0.bb.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Could anyone provide the latest package to support&amp;nbsp;the latest&amp;nbsp;se05x recipe (se05x_4.0.0.bb) ? thanks!&lt;/P&gt;</description>
      <pubDate>Sun, 24 Apr 2022 10:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/about-the-latest-SE05x-MW-file/m-p/1448185#M775</guid>
      <dc:creator>tiger_gao</dc:creator>
      <dc:date>2022-04-24T10:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: about the latest SE05x_MW file</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/about-the-latest-SE05x-MW-file/m-p/1448392#M776</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/105805"&gt;@tiger_gao&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Referring to the comments inside, looks like it is a general script which can be used for any version of MW, please kindly refer to the following for details.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1650874645543.png" style="width: 713px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177846iCCE57E421A737E8E/image-dimensions/713x180?v=v2" width="713" height="180" role="button" title="Kan_Li_0-1650874645543.png" alt="Kan_Li_0-1650874645543.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please kindly let me know if there is any further issue.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 08:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/about-the-latest-SE05x-MW-file/m-p/1448392#M776</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-25T08:25:55Z</dc:date>
    </item>
  </channel>
</rss>