<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure Authentication中的主题 Re: SE050 is unresponsive while running &amp;quot;se05x_InjectCertificate&amp;quot;</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1440336#M757</link>
    <description>&lt;P&gt;I have some building issues related to plug and trust middleware pack.&lt;/P&gt;&lt;P&gt;Is there anyway i can dirctly call&lt;/P&gt;&lt;P&gt;* sss_key_object_init&lt;/P&gt;&lt;P&gt;* sss_key_object_allocate_handle&lt;/P&gt;&lt;P&gt;* sss_key_store_set_key&lt;/P&gt;&lt;P&gt;in any project. &amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 07:39:07 GMT</pubDate>
    <dc:creator>nidhintomy</dc:creator>
    <dc:date>2022-04-07T07:39:07Z</dc:date>
    <item>
      <title>SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437581#M749</link>
      <description>&lt;P&gt;I imported source file and header file in "se05x_mw_v04.01.01\simw-top\demos\se05x\se05x_InjectCertificate" to "GetMinimal" project and called "&lt;SPAN&gt;ex_sss_entry()".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The project successfully build, but on running it gets unresponsive after reaching "sss_key_object_allocate_handle()".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Can you help me to resolve the issue?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 09:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437581#M749</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-04-01T09:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437860#M750</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194348"&gt;@nidhintomy&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you debugging the MW based on Microsoft Visual Studio ? If yes, why not directly run the project of&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;"se05x_InjectCertificate"? You just have to set up this project as a startup project like below:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1648862976756.png" style="width: 621px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/175679iAE055F5404BEBCD0/image-dimensions/621x427?v=v2" width="621" height="427" role="button" title="Kan_Li_0-1648862976756.png" alt="Kan_Li_0-1648862976756.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1648862976756.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that makes sense,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Apr 2022 01:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437860#M750</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-02T01:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437958#M751</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, I am using McuXpresso&lt;/P&gt;&lt;P&gt;I am sending apdu without applet sessions(EC key session/Aes key sessions). Is that a reason for this error.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Sat, 02 Apr 2022 08:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1437958#M751</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-04-02T08:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1439577#M754</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194348"&gt;@nidhintomy&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, maybe you didn't import the project correctly. Actually this project is cmake based, so if you are using MCUxpresso, please kindly follow the steps mentioned in&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12396.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12396.pdf&lt;/A&gt;&amp;nbsp;, especially chapter 5 - "5 Import project examples from CMake-based build system" , and change the building target to this project after import.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1649235516785.png" style="width: 717px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176045i4AE4D12B93675F58/image-dimensions/717x337?v=v2" width="717" height="337" role="button" title="Kan_Li_0-1649235516785.png" alt="Kan_Li_0-1649235516785.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1649235516785.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope that makes sense,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 06 Apr 2022 09:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1439577#M754</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-06T09:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1440336#M757</link>
      <description>&lt;P&gt;I have some building issues related to plug and trust middleware pack.&lt;/P&gt;&lt;P&gt;Is there anyway i can dirctly call&lt;/P&gt;&lt;P&gt;* sss_key_object_init&lt;/P&gt;&lt;P&gt;* sss_key_object_allocate_handle&lt;/P&gt;&lt;P&gt;* sss_key_store_set_key&lt;/P&gt;&lt;P&gt;in any project. &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 07:39:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1440336#M757</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-04-07T07:39:07Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 is unresponsive while running "se05x_InjectCertificate"</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1440978#M759</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194348"&gt;@nidhintomy&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;These are SSS APIs, and there are demos based on SSS APIs, please kindly refer to "simw-top/doc/sss/ex/doc/sss-api-examples.html" for details. For SSS API user guide, you may refer to "simw-top/doc/sss-apis.html".&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1649389306994.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176318iC751AB3F4C80B703/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Kan_Li_0-1649389306994.png" alt="Kan_Li_0-1649389306994.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1649389306994.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 03:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-is-unresponsive-while-running-quot-se05x-InjectCertificate/m-p/1440978#M759</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-08T03:42:20Z</dc:date>
    </item>
  </channel>
</rss>