<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SE050F2 version 2021 vs 2022 in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-version-2021-vs-2022/m-p/1439578#M755</link>
    <description>&lt;P&gt;What is the difference between SE050F2:&lt;/P&gt;&lt;P&gt;version 2021 with OEF ID A77E&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;version&amp;nbsp;&lt;SPAN&gt;2022 with OEF ID A92A?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I see here&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12436.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12436.pdf&lt;/A&gt;&amp;nbsp;only one column in "Table 1" with supported features for SE050F2 so it looks like the same but maybe I missed something and there are some differences? I just using SE050 to keep ec private keys and using openssl engine to using them and I wondering whether mounting different device may have impact on my implementation.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 06 Apr 2022 09:06:22 GMT</pubDate>
    <dc:creator>grzegorz2</dc:creator>
    <dc:date>2022-04-06T09:06:22Z</dc:date>
    <item>
      <title>SE050F2 version 2021 vs 2022</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-version-2021-vs-2022/m-p/1439578#M755</link>
      <description>&lt;P&gt;What is the difference between SE050F2:&lt;/P&gt;&lt;P&gt;version 2021 with OEF ID A77E&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;version&amp;nbsp;&lt;SPAN&gt;2022 with OEF ID A92A?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I see here&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12436.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12436.pdf&lt;/A&gt;&amp;nbsp;only one column in "Table 1" with supported features for SE050F2 so it looks like the same but maybe I missed something and there are some differences? I just using SE050 to keep ec private keys and using openssl engine to using them and I wondering whether mounting different device may have impact on my implementation.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 06 Apr 2022 09:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-version-2021-vs-2022/m-p/1439578#M755</guid>
      <dc:creator>grzegorz2</dc:creator>
      <dc:date>2022-04-06T09:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: SE050F2 version 2021 vs 2022</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050F2-version-2021-vs-2022/m-p/1440953#M758</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196301"&gt;@grzegorz2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Besides OEF ID, the default platformSCP keys and&amp;nbsp;&lt;SPAN&gt;the intermediate CAs are also changed. I think you have to&amp;nbsp;take care at least for the different default PlatformSCP keys when you&amp;nbsp;switch between the SE050F variants. The changed OEF ID and changed intermediate CA for cloud connectivity most likely will not have any impact&amp;nbsp;for your implementation.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 03:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050F2-version-2021-vs-2022/m-p/1440953#M758</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-04-08T03:02:12Z</dc:date>
    </item>
  </channel>
</rss>