<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SE050 Dev Board - Communication via NFC in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1436982#M746</link>
    <description>&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;by following the information on&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12395.pdf," target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12395.pdf,&lt;/A&gt;&amp;nbsp;Section 4.4.1, I was able to read the OM-SE050ARD.&lt;/P&gt;&lt;P&gt;It reads it as unknown IC with OS Javacard.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
    <pubDate>Thu, 31 Mar 2022 10:08:54 GMT</pubDate>
    <dc:creator>albertobattistello</dc:creator>
    <dc:date>2022-03-31T10:08:54Z</dc:date>
    <item>
      <title>SE050 Dev Board - Communication via NFC</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1024007#M220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the SE050 Dev Board be tested via NFC. We want to communicate with the SE050 via a Android Smartphone via NFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 17:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1024007#M220</guid>
      <dc:creator>julian_sauer</dc:creator>
      <dc:date>2020-03-12T17:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Dev Board - Communication via NFC</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1024008#M221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the Dev Board supports NFC interface via J6 and J7 jumper settings. Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103082iE00629126CFC8819/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103137iF1DEABEFC3030DC4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;but&amp;nbsp;to communicate with the SE050 via a Android Smartphone, you have to build a custom App to issue the SE050 APDU commands.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12413-SE050_APDU_specification.pdf" title="https://www.nxp.com/docs/en/application-note/AN12413-SE050_APDU_specification.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12413-SE050_APDU_specification.pdf&lt;/A&gt;&amp;nbsp; and&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/UM11225.pdf" title="https://www.nxp.com/docs/en/user-guide/UM11225.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM11225.pdf&lt;/A&gt;&amp;nbsp; for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 04:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1024008#M221</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-03-13T04:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Dev Board - Communication via NFC</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1436971#M745</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a OM-SE050ARD,&lt;/P&gt;&lt;P&gt;I have set jumper J6 to 2-3 and J7 to 2-3.&lt;/P&gt;&lt;P&gt;I have installed the NXP TagInfo app version 4.25.4 on my Samsung smartphone (which can read other NFC tags).&lt;/P&gt;&lt;P&gt;However, when approaching the OM-SE050ARD antenna to the phone, nothing happens. Is this a problem with the smartphone app not sending the APDUS or do I need to program something into the SE050?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 09:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1436971#M745</guid>
      <dc:creator>albertobattistello</dc:creator>
      <dc:date>2022-03-31T09:54:17Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 Dev Board - Communication via NFC</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1436982#M746</link>
      <description>&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;by following the information on&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12395.pdf," target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12395.pdf,&lt;/A&gt;&amp;nbsp;Section 4.4.1, I was able to read the OM-SE050ARD.&lt;/P&gt;&lt;P&gt;It reads it as unknown IC with OS Javacard.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 10:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-Dev-Board-Communication-via-NFC/m-p/1436982#M746</guid>
      <dc:creator>albertobattistello</dc:creator>
      <dc:date>2022-03-31T10:08:54Z</dc:date>
    </item>
  </channel>
</rss>