<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SE050 - GPIO usage in Secure Authentication</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1424440#M718</link>
    <description>&lt;P&gt;Hello Kan,&lt;/P&gt;&lt;P&gt;thanks for the quick reply. Unfortunately I would use the GPIO as an input :-/. But I look into the AN for more informations.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Sascha&lt;/P&gt;</description>
    <pubDate>Tue, 08 Mar 2022 08:54:45 GMT</pubDate>
    <dc:creator>SaschaH</dc:creator>
    <dc:date>2022-03-08T08:54:45Z</dc:date>
    <item>
      <title>SE050 - GPIO usage</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1423889#M716</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I looked into the datasheet of the SE050 device.&lt;/P&gt;&lt;P&gt;Two Pins in package are marked as GPIO pins. Can they only be used in context to&amp;nbsp;ISO7816? Are there any informations available if they can be used as normal GPIO? I am interested in a path for a direct alarm trigger input.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sascha&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 11:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1423889#M716</guid>
      <dc:creator>SaschaH</dc:creator>
      <dc:date>2022-03-07T11:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 - GPIO usage</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1424216#M717</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197802"&gt;@SaschaH&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you referring to IO1 and IO2? Actually they can also be used as&amp;nbsp;I2C Master interface for&amp;nbsp;the Sensor/Actuator use case as described in AN12449(&lt;A href="https://www.nxp.com/docs/en/application-note/AN12449.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12449.pdf&lt;/A&gt; ), but they&amp;nbsp;&lt;SPAN&gt;can not be used as GPIO.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In case you would like to control a GPIO via the middleware you have to connect the device with an I2C-bus I/O expander and follow the cases mentioned in AN12449.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope that makes sense,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 02:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1424216#M717</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-03-08T02:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 - GPIO usage</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1424440#M718</link>
      <description>&lt;P&gt;Hello Kan,&lt;/P&gt;&lt;P&gt;thanks for the quick reply. Unfortunately I would use the GPIO as an input :-/. But I look into the AN for more informations.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Sascha&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 08:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/SE050-GPIO-usage/m-p/1424440#M718</guid>
      <dc:creator>SaschaH</dc:creator>
      <dc:date>2022-03-08T08:54:45Z</dc:date>
    </item>
  </channel>
</rss>