<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Secure AuthenticationのトピックSe050-PLUG-TRUST-MW empty &amp;quot;axCi_Mutex&amp;quot; implementation and possibly deadlock in NXP code</title>
    <link>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1408961#M698</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'am using MW version 03.03.00&lt;/P&gt;&lt;P&gt;I found out that openssl plugin uses mutex which has empty implementation in the file "sss/plugin/openssl/engine/src/ax_cryptoIpc.c" is it required to add implementation? Another issue with this mutex is that with proper implementation it can cause deadlock because of the bug in the file "sss/plugin/openssl/engine/src/ax_sssEngine_ecc.c". There is a code like this:&lt;/P&gt;&lt;P&gt;axCi_MutexLock();&lt;/P&gt;&lt;P&gt;if (status != kStatus_SSS_Success) {&lt;/P&gt;&lt;P&gt;return NULL;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;axCi_MutexUnlock();&lt;/P&gt;&lt;P&gt;mutex is not released in case of error and application will be deadlocked after next function call&lt;/P&gt;</description>
    <pubDate>Fri, 04 Feb 2022 10:51:38 GMT</pubDate>
    <dc:creator>grzegorz2</dc:creator>
    <dc:date>2022-02-04T10:51:38Z</dc:date>
    <item>
      <title>Se050-PLUG-TRUST-MW empty "axCi_Mutex" implementation and possibly deadlock in NXP code</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1408961#M698</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'am using MW version 03.03.00&lt;/P&gt;&lt;P&gt;I found out that openssl plugin uses mutex which has empty implementation in the file "sss/plugin/openssl/engine/src/ax_cryptoIpc.c" is it required to add implementation? Another issue with this mutex is that with proper implementation it can cause deadlock because of the bug in the file "sss/plugin/openssl/engine/src/ax_sssEngine_ecc.c". There is a code like this:&lt;/P&gt;&lt;P&gt;axCi_MutexLock();&lt;/P&gt;&lt;P&gt;if (status != kStatus_SSS_Success) {&lt;/P&gt;&lt;P&gt;return NULL;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;axCi_MutexUnlock();&lt;/P&gt;&lt;P&gt;mutex is not released in case of error and application will be deadlocked after next function call&lt;/P&gt;</description>
      <pubDate>Fri, 04 Feb 2022 10:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1408961#M698</guid>
      <dc:creator>grzegorz2</dc:creator>
      <dc:date>2022-02-04T10:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: Se050-PLUG-TRUST-MW empty "axCi_Mutex" implementation and possibly deadlock in NXP cod</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1410110#M699</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196301"&gt;@grzegorz2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Actually I didn't find such kind of issue in the latest version of&amp;nbsp;04.01.01, would you please update the MW on your hands? or is there any reason to stay with the older version? Please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se051-proven-easy-to-use-iot-security-solution-with-support-for-updatability-and-custom-applets:SE051?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se051-proven-easy-to-use-iot-security-solution-with-support-for-updatability-and-custom-applets:SE051?tab=Design_Tools_Tab&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 08:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1410110#M699</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2022-02-08T08:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Se050-PLUG-TRUST-MW empty "axCi_Mutex" implementation and possibly deadlock in NXP cod</title>
      <link>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1410273#M700</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I downloaded this new version and I don't see these mutexes anymore so I will use it. Thanks for support.&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 12:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Secure-Authentication/Se050-PLUG-TRUST-MW-empty-quot-axCi-Mutex-quot-implementation/m-p/1410273#M700</guid>
      <dc:creator>grzegorz2</dc:creator>
      <dc:date>2022-02-08T12:25:32Z</dc:date>
    </item>
  </channel>
</rss>